Part Number: DLP2010NIR Other Parts Discussed in Thread: DLP650LNIR , DLP4500NIR Hi E2E, Good day.
Our customer has the specifications of the following laser:
1. Nanosecond, duration: 10-250 ns, 1-100 kHz, wavelength: 1064 nm, max power: 20 W; 2. Picosecond…
Part Number: DLP2010NIR Other Parts Discussed in Thread: DLPC150 , DLPC3470 , DLP2010LC , DLPC-API Hello Team,
Good day.
My customer is trying to use DLP2010NIR using Labview over USB. Do we have an example code for this?
Regards,
Renan
Part Number: DLP2010NIR Hello,
I have read in the documentation that NIR NANO EVM does a black reference measurement before every sample scan by turning off all the mirrors. Then subtracts the dark current from the sample spectrum. So, I wanted to know…
Part Number: DLP2010NIR Hi all,
Is the DLP2010NIR (DLP Technology) is valid by EPA ( environmental protection agency )?? From the attachment (evaluation module ), I have found that gives the application in water quality testing, so how to find its certified…
Part Number: DLP2010NIR Dear All,
I would like to know if it is possible to have the diffraction efficiency plot for the DLP2010NIR.
Thank you in advance.
Best regards,
Astghik
Part Number: DLP2010NIR Other Parts Discussed in Thread: DLPC150
Hello Everyone ,
My application calls for straightforward use of the DMD . I would like to have the micromirrors in a fixed position and that's it.
I shall be supplying Vss , Vdd ,…
Part Number: DLP2010NIR Other Parts Discussed in Thread: DLPC150 , DLP2010 , DLPA2005 , , TIDA-00554 Hello everyone,
I recently bought DLP2010NIR (DMD), DLPC150 (controller) and DLPA2005 (driver). My purpose is to put all the DMD of DLP2010NIR on -17° to…
Guangning,
Going back to your original question, the DLPC150 chipset which supports the DLP2010NIR may be able to perform the function you are looking for but it is not supported in the given EVM for this chipset (which is tailor-made for spectroscopy…
Part Number: DLPC150 Other Parts Discussed in Thread: DLP2010NIR , , DLPA2005 I am trying to get 2880 Hz binary pattern display using 24-bit parallel with the dlpc150 and dlp2010nir. In section 8.1 of the DLPC150 datasheet "Pattern Generation Mode" is described…
Part Number: DLP2010EVM-LC Dear All,
I would like to purchase the DLP2010EVM-LC which works with DLP2010 VIS DMD. I will be removing the Optical engine and simply shoving light onto the DMD. However, I am working with NIR and would like to know if it is possible…