Hello Geoffrey,
Since you are attempting to use the DLP2021LEQ1EVM, the root of the problem is that you must import the new DLP2021-Q1 Composer Project and FPGA Configuration ( DLPC153.ZIP) DLP Composer project specific to the DLP2021-Q1 into DLP Composer 15…
Hello Yuan,
Responding to your questions:
1) Yes, you can change the projection pattern by updating the start address and the number of frames fields. If you are using the address values provided from the user's guide or example code, the address may…
Hi Xu,
Is distance between the projector and surface between 850-1150mm? This is the focal range of the DLP2021-Q1 EVM.
Can you also take a photo of the lens cavity at the front of the projector? It appears as though a lens is missing or has shifted.…
Hi Martin,
The DLP2021-Q1 FPGA design should release to TI.com later this month. The DLP3021-Q1 design is already released to TI.com. It is available at this link: https://www.ti.com/lit/zip/dlpc135
The FPGA design is released with the Composer project…
Part Number: DLP2021LEQ1EVM Tool/software: Hi,
I'm having trouble rebuilding the DLP Composer project provided in DLP2021-Q1_DGP_RGB_60Hz.zip — 504041 K . I get the below errors when rebuilding.