The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: DLP2021LEQ1EVM Other Parts Discussed in Thread: DLP3021LEQ1EVM , DLP3021-Q1 , DLPC120-Q1 Tool/software: Dear all. I have a few inquiries regarding DLP2021LEQ1EVM that I would like to ask:
1. According to the User Guide, it is mentioned that…
Part Number: DLP2021LEQ1EVM Tool/software: I'd like to replace a current image/video stored on the onboard flash with a different version without having to program the entire flash memory. This seems to be possible given the DLP Composer Flash Programming…
Part Number: DLP2021LEQ1EVM Tool/software: Hi,
I'm having trouble rebuilding the DLP Composer project provided in DLP2021-Q1_DGP_RGB_60Hz.zip — 504041 K . I get the below errors when rebuilding.
Hi Ryu,
Sorry for the delay, I just received the information from our internal team. Please see the SPI commands that using the SPI Flash in the attachment.
Also, you should refer to the MCU datasheet to get the information for needed registers.
…
Part Number: DLP2021LEQ1EVM Tool/software: Hello, I was wondering what it could mean if the racecar video just stopped working.
We have flashed the firmware several times, and have updated the offset accordingly. We followed the videos to the best of…
Part Number: DLP2021LEQ1EVM Tool/software: Hello my future savior,
I have a trouble with playing a 16s video on DLP2021LEQ1EVM.
The total play time is 16s long but I only can watch the front 8s of the video. (The video size is about 27MB.)
Is there any…
Part Number: DLP2021LEQ1EVM Tool/software: Hello, I have a DLP2021LEWQ1EVM kit with everything. I installed everything on the pdf file all the drivers and the DLP Control Program and DLP Composer. On the connection tabs of the DLP Control I can connect…
Part Number: DLP2021LEQ1EVM I purchased 3 DLP2021LEQ1EVMs. When I projected the image, a thin vertical ghost ghost appeared on the left side of the image. It doesn't appear on a specific image, it appears on all images. This is the same phenomenon for…
Part Number: DLP2021LEQ1EVM
I purchased DLP2021LEQ1EVM. The User’s Guide says “Please refer to the EVM bill of materials to review the temperature specifications of all components used in the EVM design.” However, I do not know how to obtain the BOM.…
Hi Kalaivani,
Ensure the EVM switches are set to the "Host Mute" mode when attempting to send commands from your external NXP S32 controller.
The 5MHz is valid.
CPOL and CPHA must both be '0' (defined as Mode 0) where data is sampled at the leading…