Part Number: DLP3010 Hi Experts,
We are designing a projection system around DLP3010 for a medical device. We require quite a large amount of power trasmittance from a 894nm VCSEL array. Current estiamtes at the DMD are an average irradiance of ~500mw…
Part Number: DLP3010 Other Parts Discussed in Thread: DLP230GP , , DLP2010 Tool/software: Hi,
We are looking to evaluate these three DMD DLP2010, DLP230GP and DLP3010 along with the Dev kit DLPDLCR3010EVM-G2 for a specific projection system to determine…
Part Number: DLP3010 Tool/software: Hi,
I am planning to use DLP3010 in one of my products which has an operating temperature specification of -20 deg C to +70 deg C.
As the operating temperature for DLP3010 is 0°C to 70° C, I am concerned about the…
Part Number: DLP3010 Hi everyone,
We are still using a DLP3000. It's (finally) kicking the can and is no longer responding to commands as it should. I'm looking at replacements but honestly there are way too many options.
For reference, we removed…
Part Number: DLP3010 Tool/software: Hi everyone,
I’m looking for the full software suite for the DLP3000–the GUI, drivers, and SDK. TI support has been unwilling to provide it as the device is too old and shouldn’t be developed on, according to them…
Part Number: DLP3010 Tool/software: Hello Experts,
I downloaded the STEP file (see image 01) for DLP3010 and it is not quite what I am looking for. I am looking for a model similar to the image 02 below but with the DLP3010 spec.
Can you please check…
Part Number: DLP3010 Tool/software: Could you please provide me with the thermal and mechanical material properties for the DLP 3010? We are building our thermo-mechanical model which incorporates DLP.
Thanks
Part Number: DLP3010 Tool/software: Hi,
We are planning to design and integrate a dental Intra-oral scanner based on triangulation and structured light methods, utilizing a DLP projector system.
I have reached out to some of the partners listed in…
Part Number: DLP3010 Tool/software: Hello, I am conducting experiments with the DLP3010EVM-G2 using the DLP EVM GUI, and the device selection in the GUI was set to DLP3010EVM-LC. I mistakenly performed the action of writing the firmware of the DLP3010EVM…