Part Number: DLP3010 Tool/software: Hi,
I am planning to use DLP3010 in one of my products which has an operating temperature specification of -20 deg C to +70 deg C.
As the operating temperature for DLP3010 is 0°C to 70° C, I am concerned about the…
Part Number: DLP3010 Tool/software: DLPDLCR3010 and need to change its aspect ratio. While we have installed the GUI intended for this purpose, the options required for changing the aspect ratio are not visible in the interface.
For your reference, I…
Part Number: DLP3010 Tool/software: Hello TI team,
We have mentioned this problem last time, but recently we have similar problems, that is, there are bright spots or vertical lines on the DMD screen. Our workshop has already done ESD protection, including…
Hi Soren,
1D Keystone : allows adjustments in pitch(angle up/down), throw ratio(distance from wall/screen size), vertical offset(offset up/down from projector optics). This is supported by the DLP3010G2-EVM
2D Keystone: allows adjustments in pitch, yaw…
Part Number: DLP3010 Tool/software: Hello, Ti team.
Our company produces DLP optical machines and has considerable industry experience.
As we all know, DMD is easy to be damaged and produce bad points.
There are many reasons for production, such as static…
Part Number: DLP3010 Other Parts Discussed in Thread: , DLPC3433 , , DLPC3478 , DLPA2005 , DLPA3000 For the development of desktop dental 3D scanner, I have identified two EVM for the DLP3010. One is DLP Lightcrafter Display 3010 EVM and the other is DLP3010…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC3478 Urgent request! When the customer burned 8bite vertical stripes, set 13 pattern sets, each set set the same 6 1280x1 8-bit map, each map is a few kb, but after setting the burning, there is…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC3433 DLP3433 PCB layout guide said DMD HS signal pattern length matching is needed.
And there is below table in DLP3010 datasheet.
When I design sub-LVDS signals, is package net length have to…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC300 , DLPC3478 , DLPC3470 , , DLP2010LC I can't find where to buy the ref. DLP3000-C300REF, is it discontinued?
If so, what is its continuation? That is to say with which component could I replace…
Part Number: DLP3010 I am designing projector using DLP3010, DLP3433.
There are DMD bus high speed signals like DMD_HS_WDATA_X_P, DMD_HS_WDATA_X_N.
In my current FPCB design, those signals are crossed. So via is needed in high speed signals.
My question…