Part Number: DLP3010LC Other Parts Discussed in Thread: DLP3010 , DLPC3438 , DLPC3478 Dear TI experts,
My customer considers to change the part from DLP3010 to DLP3010LC, due to delivery issue.
I saw several E2E threads, but still i am not sure that DLP3010…
Part Number: DLP3010LC For my experiments, I need to use a laser source to illuminate the DMD, specific model DLP3010LCFQK. If I want the "projected image", i.e. the outgoing ray to be perpendicular to the DMD plane, i.e. from the normal direction of…
Hello Cem,
There are some bugs with the GUI when it comes to editing FW. We are currently working on fixing these issues.
The team will have to look into the pattern set behavior too. Thank you for your patience.
Regards,
John
Part Number: DLP3010LC Other Parts Discussed in Thread: DLPA2005 , DLPC3478 Hi Experts,
Recently I need to test the 1-bit monochrome pattern display with DLP3010LCFQK working in external pattern streaming mode.
The DLPC Write Pattern Configuration (96h…
Hello Gabriel,
John will coordinate with you through direct messages. Since this thread appears to be nearing its end, I will close it.
Thank you for your business!
Kind regards,
Austin
Part Number: DLP3010LC Hi,
I was wondering if anyone knew where to source connectors to connect to the FQK Package 57-Pin LGA on the DLP3010LC DMDs.
I would like to design a custom FPC cable and board to implement in our design.
Thank you,
Justin
Part Number: DLP3010LC Other Parts Discussed in Thread: DLPC3478 , DLPA2005 Dear Expert
We found the problem using the firmware provided, so we need to modify it. Since our scene is light controlled, we are powered by lithium batteries. Leds are frequently…