Hi Mayank,
My DLP3010LC-EVM have broken and does not work.
So whether TI can reproduce the case on a DLP3010LC-EVM.
I test DLP3010 and DLP3010LC. They both could reproduce the same issue on my board with BLUE_LED_ONLY firmware based on version 8.0.0. …
Hello Lee,
Can you confirm that the optical engine has a DLP3010 and not a DLP3010LC ? If this is the case, the DLPC3478 will reject the DMD as it is meant to be used with the DLP3010LC .
Regards,
Austin
Part Number: DLPC7540EVM Other Parts Discussed in Thread: DLP471TEEVM , DLP4710LC , DLP471TP , DLP471TE , DLP3010LC , DLP2010LC Hello,
I want to use DLPC7540EVM together with DLP471TEEVM as spatial light modulator. Since I don't need 4K resolution, do I have…
Part Number: DLPC3470 Other Parts Discussed in Thread: DLP3010LC , DLPC3478 , DLP3010EVM-LC , DLP2010 , DLP2010LC
Hi,
We are currently developing DLPC3470 custom display board while checking the reference design for the evaluation board DLP2010EVM-LC.
While…
Part Number: DLP3010 Hello everyone,
I have encountered some trouble in long-term using DLP3010 projector according to DLP3010LC-EVM.
When working with trigger in mode by a camera or other controller, at first, the DLP3010 display is normall and Trig2_out…
Part Number: DLPC3470 Other Parts Discussed in Thread: DLPC3430 , DLP2010 , DLP2010LC , DLP3010 , DLP3010LC Hi
We are now using DLP2010 for 3D AR application
Can both DLPC3470 and DLPC3430 be used for DLP2010 ?
Can you share what is the difference between DLPC3470…
Hello Josel,
We do not have a documented procedure for removing DMD or optical engine from the EVM. However, this method should be straight forward with a Philip screwdriver and a blade to cut sealant.
Few suggestions -
Please review the mounting concept…
Hello Cooper ,
Could you please confirm that system has correct DMD? The DLPC3478 controller works only with DLP3010LC DMD (DLP3010LCFQK).
www.ti.com/.../DLP3010LC
The firmware checks for the correct chipset combination and also ensures that they connected…
Hello Sun,
The DLP3010AFQK DMD is not a supported chipset option for DLPC3478 controller. The DLPC3478 controller works with only DLPC3010LC DMD (DLP3010LCFQK).
https://www.ti.com/product/DLP3010LC
If you are using optical engine from a third-party supplier…
Hi Austin,
Their experiment needs the DMD to be exposed to visible light and then manipulate the mirrors in the DMD to get reflections only from a particular row or column but the DMD is covered by a heat sink and facing inwards. So they need to extract…