Hi Austin,
Their experiment needs the DMD to be exposed to visible light and then manipulate the mirrors in the DMD to get reflections only from a particular row or column but the DMD is covered by a heat sink and facing inwards. So they need to extract…
Part Number: DLPA3000 Other Parts Discussed in Thread: DLPA3005 , DLP3010LC , DLPC3478 , Dear ,
I use DLP solution DLPC3478 + DLP3010LC + DLPA3000, I want to increase power driver, May I use DLPA3005 instead of DLPA 3000 directly ?
Hello Okra,
Can you clarify what DMD you have for this design? The DLP3010 and DLP3010LC are different DMDs and you have the DLP3010 as a listed part above.
Regards,
John
Hello Constanza,
Welcome to DLP forum and thank you for your interest in DLP technology.
Are you referring to the DLP3010EVM-LC evaluation module?
https://www.ti.com/tool/DLP3010EVM-LC
This is an evaluation module and it does includes complete chipset…
Hello Morgan,
Thank you for providing the part numbers. These two DMDs, although similar, are meant for two distinct platforms. The DLP3010 is designed to be used with a DLPC3433/3438 controller for display applications. The DLP3010LC is meant to be used…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLP3010 , , DLPA2005 , DLP3010LC Dear TI,
Project description: DLPC3478+DLPA2005+DLP3010. The attached file is hardware schematic diagram,please review it. The software has been successfully…
Part Number: DLPA2005 Other Parts Discussed in Thread: DLP3010LC , DLPC3478 , , DLP3010EVM-LC Hello, TI experts.
The main purpose of the letter is to seek some assistance.
We built the circuit ourselves, the configuration used is DLPC3478+DLPA2005, and the…
Chris,
I was able to find a link and download DLP3010LC GUI v2.2.0.6 from TI. However this gives me the same "EVM type cannot be recognized" error that the latest version does. K eep in mind, I am trying to create customized firmware using the…
Hi Mayank Khandelwal.
Jiahui Gao posted a question on my behalf.
DMD is DLP3010LC.
CMD is normally transferred from the external MCU to the DLPC3478.
What more should I check?