Part Number: DLP3021LEQ1EVM Hi Sir,
OS : Win10 Home Edition 21H2 64 bits
I have download and install FTDI D2XX driver then run "DLP Control Program 15.1.0.26".
But "SPI" interface did not appear in command interface.
Could anyone help me to…
Part Number: DLP3021LEQ1EVM Hello!
What options for sending a 2D pattern are there in the DLP3021 LEQ1EVM? To send a 2D pattern , do I need to change the FPGA firmware ?
I need black and white static 2D patterns of several pixels with mirrors on and…
Part Number: DLP3021LEQ1EVM Other Parts Discussed in Thread: DLP3021-Q1 Good day!
Please tell me if the DLP3021LEQ1EVM demo board has triggers for controlling ( synchronizing ) external devices ? Input trigger from an external device.
Input sync trigger…
Part Number: DLP3021LEQ1EVM Other Parts Discussed in Thread: MSP430G2553-Q1 , DLP3021-Q1 , DLPC120-Q1 Hello!
How to view signals on pins of Xilinx chip in DLP3021LEQ1EVM demo board via Code Composer ? Does SPI programmer make FPGA debug ?
Yours faithfully…
Part Number: DLP3021LEQ1EVM Hello,
I`m trying to communicate to the DLP3021LEQ1EVM via SPI in mute Host mode and when sending frames with the SPI protocol and the frames provided in the FPGA users guide I receive no response.
For example in order…
Part Number: DLP3021LEQ1EVM Other Parts Discussed in Thread: DLP3021-Q1 , MSP430G2553-Q1 Hello!
Tell me, please: 1. Can DLP3021LEQ1EVM be used as a monochrome micromirror control system ( without RGB LEDs)?
2. Is it possible to set a constant static…
Part Number: DLP3021LEQ1EVM Other Parts Discussed in Thread: MSP430G2553-Q1 Hello!
What is the function of EEPROM in EVM ? Is it a necessary matching component for MCU or FPGA? Thanks!
Best regards,
Part Number: DLP3021LEQ1EVM Other Parts Discussed in Thread: MSP-FET
Hello!
1. Why does the DLP3021LEQ1EVM demo board need an external Cheetah SPI Host Adapter "F" ?
2. What is the part number for the Cheetah SPI Host Adapter? The DEF060A adapter…
Part Number: DLP3021LEQ1EVM Hello.
What is the brand / size power connector for the DLP3021LEQ1EVM demo board?
What is the voltage and current for the external power adapter of the DLP3021LEQ1EVM demo board? (the document indicates 12V, as well as…
Part Number: DLP3021LEQ1EVM Hi,
My customer designed the board with reference to the DLP3021LEQ1EVM.
The EVM's BOM list includes FPGA (XA7S15-1CPGA196Q)
However, this part is not currently available to customer. So he is trying to use a part of…