Part Number: DLP3030Q1EVM Hi,
We have bought 2 sets of DLP3030Q1EVM, and connected all parts, including DMD board, R\G\B LED and PC, according to the User Guide. We can see the image from the DMD chip and get the data from the EVM through the ACP. Unfortunately…
Part Number: DLP3030Q1EVM Dear All,
As we know,"Maximum power can also depend on how well optimized the calibration routine was and the calibration data that was flashed onto the system. "
I want to know how to optimize the calibration routine…
Part Number: DLP3030Q1EVM Other Parts Discussed in Thread: TMS320F28027
Dear T eam ,
Due to the shortage of DLP3030Q1EVM , we are planning to produce our own EVM.
Is the .ccxml for XDS100 also compatible with XDS200?
I encountered the following error when…
Part Number: DLP3030Q1EVM HI,
I want download DLPC120 Control Program ,but i can just find the DLPC120 Automotive Control Program Lite 1.3.1.41.
Where can i get the f ull version of DLPC120 ACP?
Thanks!
Part Number: DLP3030Q1EVM Other Parts Discussed in Thread: DLP3030PGUQ1EVM Dears,
This is Taiwan OFILM Hardware engineer Weite.
We had buy one DLP3030Q1EVM(develop PGU optical engine)
In the DLPC120ACP, the R/G/B current Duty (LDC Index) settings are…
Part Number: DLP3030-Q1 Hello Guys,
I have the similar questions about safety critical application of DLP3030-Q1. Could you provide technical support on related issues?
Part Number: DLP3030Q1EVM
Hi Experts,
Seeking your advise for this query I posted on behalf of my Cx:
"If I provide the EVM with HDMI input from a laptop or pc on a duplicate screen setting, I am getting the display output, but while I provide it 720p…
Hi Sundar -
The best way to determine if the DLPC120 can handle specific blanking periods is to simply test it with a physical setup. Do you have an existing setup?
The Parallel Interface Supported Resolutions table from the DLPC120-Q1 datasheet only provides…
Part Number: DLP3030Q1EVM We have received a DLP3030Q1EVM circuit board. I used a software(DLPC120 Autotive Control Program 1.4.2.58) to adjust it, but now the total power is only 2.88(W)(0.24A X 12V).I want to know how I can use this software (DLPC120…
Part Number: DLP3030Q1EVM We have received a dlp3030q1evm circuit board making document and schematic diagram document, version D. I want to know whether it is normal to turn on the red light before burning the software? If normal, what program do I need…