Part Number: DLP4500 Hi TI experts,
I am trying to present short monochrome videos using my DLP4500EVM. I would prefer not to stream them from a computer (instead store in flash memory?), and I would really like to trigger them using an Arduino or a NIDAQ…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: DLP4500 , DLPC350 Hi, apologies in advance, I have very little exposure to dlp products, so some terms and concepts are new to me, and my questions might be naive.
My goal is to download patterns…
Part Number: DLP4500 Other Parts Discussed in Thread: DLPC350 Hi, We have been using DLPC350 firmware v3.1.0 with the DLP4500FQE for many years and it has been working well. (The firmware we use on the DLPC350 is based on DLPR350PROM_v3.1.0.bin with out custom…
Part Number: DLP4500
Hello E2E,
Regarding the DLP4500 ( https://www.ti.com/lit/ug/dlpu011f/dlpu011f.pdf?ts=1640106955868 ) there is a detail provided for RGB illuminators in this module. Do we provide illuminator options with NIR as well?
Also, can you…
Part Number: DLP4500 Hi,
I was wondering if anyone would be able to help me with an issue that I'm having. I'm currently using Matlab to generate some patterned masks, which are then sent over HDMI to the Wintech PRO4500. The issue that I'm having is…
Part Number: DLP4500 Other Parts Discussed in Thread: DLPC350 , Hi team, I received the following question at one of my accounts:
Product: LightCrafter 4500 Evaluation Module (DLP4500, DLPC350)
Scenario: Firmware-Upgrade/Upload with “DLP LightCrafter 4500…
Part Number: DLP4500
Use an external signal to trigger 4500 projection. There is no problem when the external signal is detected. At present, the DLP does not process the external input trigger signal. How can I solve this?
Part Number: DLP4500 I am having problem with the locking of HDMI signals. Signals are detected but Signal Status is stuck in "Processing". The most likely cause is that both Horizontal and Vertical Resolutions are off by 1 or 2. For example…
Part Number: DLP4500 Other Parts Discussed in Thread: DLPC350 I want to know whether the dlp 4500evm can connect raspberry pi 4 model B.
Pi4 has hdmi and usb so if I can connect them with dlp 4500 evm