Part Number: DLP4500-C350REF Dear TI geniuses:
Why under the pattern sequence mode, the displayed pattern doesn't look colorful to the human eye as under the video mode? It is in grey under pattern sequence mode.
thanks!
Hi Danilo,
Below is the current implementation of the buffer which is internal to the DLPC350. I am not sure if everything can be reconfigured to work with an external system such as a beagle bone board.
Is the customer following this reference design…
Hello Kokoro-san,
The "DLP4500-C350Ref High Resolution, Portable Light Steering Reference design using DLP technology" is based on the DLP4500 EVM.
https://www.ti.com/tool/DLP4500-C350REF
Could you please review the design files (brd file stored…
Hi Marvin,
Initially looking through documents I do not see anything related to those screws. In the EVM user guide it does mention that iView developed the light engine so I would assume they would know the screw size.
There is also this reference…
Hi User,
Can you please provide the link address you mentioned has expired?
The design files for the DLPLCR4500EVM can be found here: https://www.ti.com/tool/DLP4500-C350REF .
Please let us know if that is the one you are looking for.
Regards,
Lori
Hello Fujiwara-san,
DLP4500 GUI works with DLPC350 controller. You need to build the drive electronic board based on DLPC350. Please refer to the block diagram in page 9 of the DLP4500 EVM user guide
https://www.ti.com/lit/ug/dlpu011f/dlpu011f.pdf
The…
Hello Ninghan,
Generally speaking you will need to re-establish contacts between the port and the board. The piece should fit on top of the pads somewhat intuitively. The schematic for the EVM can be found on the DLP4500-C350REF page . Be sure that all…
Hi Ray,
If you have the soldering resources available you could replace the HDMI connector on the board.
you can find a BOM for this EVM in the reference design here https://www.ti.com/tool/DLP4500-C350REF
Best regards,
Arthur Brown
Matthias,
J11.4 is used as the input to Vcca of the voltage translator. I recommend reviewing the schematic associated with the EVM reference design here for more information.
https://www.ti.com/tool/DLP4500-C350REF
I hope this helps.
Best Regards,
Philippe…
Part Number: DLPLCR4500EVM Hi,
(There is a relevant previous question : https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/931070/dlplcr4500evm-cad-or-drawing-file-mechanical ,
but it does not solve my question and the previous one is…