Part Number: DLP4500NIR Hello everybody
I'm setting up my own spectrophotometer in NIR region (1300-2500nm)
I just want to know from you the best way to align the optics, filter, grating, DMD, detector. My light source is a traditional tungsten bulb…
Part Number: DLP4500NIR Hello everybody,
we're operating the DLP4500NIR DMD with the controller from the DLP4500EVM, but with an external light source. When running in either Video Mode (with any of the input sources) or Pattern Mode, The output Signal…
Part Number: DLP4500NIR Other Parts Discussed in Thread: DLP4500 Hello everyone
Is it possible to reprogram the DMD to modify the tilt angle of micromirrors? How?
Thank you
Other Parts Discussed in Thread: DLP4500NIR Hi,
I have an application for beam shaping and I would like to use the DLP4500NIR. The illumination source yields powers of 2W at NIR (800nm). However, in this application, the power is not evenly distributed…
Part Number: DLP4500NIR Other Parts Discussed in Thread: DLP4500 We are testing a brand-new DLP4500NIR DMD in our Lightcrafter 4500 development kit, which we've deconstructed for structured light purposes. The stock, visible-light DLP4500 works perfectly…
Part Number: DLP4500NIR Hello everybody.
We are using the DLP4500NIR in the DLP4500EVM. I would like to know if there is a way to control the framerate at which the DMD mirrors are refreshed when operated in video mode.
Thanks,
Tim
Daniel,
If you look at the datasheet for the DLP4500NIR and the schematic for the Lightcrafter, you'll see that the pin-outs are not the same, which means that the flex is not just a straight through flex and you will not get desired operation on the…
Other Parts Discussed in Thread: DLP4500NIR I am using a broadband light source to illuminate a dlp4500NIR. I have read the spec sheet showing the transmission curve for the windows, which are optimized for the 700 nm - 2500 nm range. Most of my light…
Other Parts Discussed in Thread: DLP2010NIR , DLPC150 , DLPC350 , DLP4500NIR , DLP4500 Hi there,
I am interested in the application of DMD at NIR range (1-2.5um). I have found DLP2010nir and DLP4500nir with there controller dlpc150 and dlpc350 respectively…
Other Parts Discussed in Thread: DLP4500NIR , DLP4500 Hi,
I have some questions about DLP4500 and DLP4500NIR.
1. What is the scan rate?
2. Do you have Soil scan samples?
3. What is the spot size of sample area?
4. What wavelength resolution…