Part Number: DLP470TP
I am looking for an end-product which will have the option to be able to switch between 60,120,144 or 240hz 1080p or 4K@60Hz.
Will the DLPC itself be enough to add this functionality or will the FPGA firmware need to be rewritten…
Part Number: DLP470TE Hi, I want to know if the DLP470TP or the DLP470TE chipsets can support 4K UHD (3840 × 2160) resolution at native 24hz/48hz/50hz frame rate without 3:2 pulldown. The product tech sheets claims the chips has a refresh rate of…
Part Number: DLP470TP It is marked as "LIFEBUY" http://www.ti.com/product/DLP470TP
But it is new and hadn't even started selling to non-OEM partners.
Yet the DLPC6421 controller for it is marked as "ACTIVE" http://www.ti.com/product…
Part Number: DLP470TP Required tolerances and other stuff such as preferred materials (based on durability, heat resistance, etc), where can I find this?
I already understand we can get the ribbon cable connecting the DMD to the PCB made by some general…
Part Number: DLP4710 Dear all
In the DLP470TP datasheet and DLP4710 datasheet, the Micromirror Pitch of both are 5.4-µm, Diagonal Micromirror Array of both are 0.47-Inch, but why does DLP470TP support 4K,but DLP4710 only support 1080p ?
Part Number: DLP470TP Understand that, TI recommend the RTIR with refractive index(RI) about 1.70. However, most of the refractive index of RTIR in the market is about 1.50.
My client and I would like to know,
1. What is the effect to DLP performance…
Part Number: DLP470TP The Optical Module Manufacturer partners of TI do not offer specific components of DLP optical engines such as TIR prism, flyeye lens, LED collimation lens, dichroic mirrors and projection lenses, but we are building our own optical…
Part Number: DLP470TP Hi, I'm an Optical Engineer working on the Illumination optics design for a client. I received a document about DMD Etendue for DLP470TP. (DMDEtendue) from my client.
I need to get some confirmation base on the information provided…
Part Number: DLP470TP So on the product page of DLP470TP it says "Samples: Not Available" and "Order Options: Contact Distributor " unlike other ACTIVE DMDs where distributors such as TI, Digikey and Mouser are directly listed. When I click…
Part Number: DLP470TP What latency can be expected from the DLPC6421 and DLP470TP? Of course the video backend chip which will convert HDMI or DIsplayPort video to LVDS will introduce its own latency, but I want to know the latency of DLPC6421 and DLP470TP…