Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLP4710
please provide me the link from where i can order this FLASH FPC cable (LH90) of the DLP4710 EVM-LC
Hello User,
Welcome to the E2E forum and thank you for your interest in DLP® technology.
To start I might recommend that you consider the DLPC3439/DLP4710 display platform . This is similar to the DLPC3479/DLP4710-LC (light control) EVM that this…
Part Number: DLP4710EVM-LC Dear Madam or Sir,
Realated to the last question, I hope to control the LED PWM to change the output of LED(R,G, B)., and Now I use I2C to control this.
As I understand on the <Programe Guide>
When I use the following…
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLP4710 , DLPC3479 Tool/software: Hi,
I want to use my DLP4710 Light Control chipset in external pattern mode, to display 1-bit patterns with an exposure time of at least 1 second (maybe 2…
Part Number: DLP4710EVM-LC Tool/software: Dear Technical Support,
We have recently updated the firmware to version 8.4.0 and are using GUI version 3.2.0.7. When using the Light Control Tab under Internal Patterns to project 17 horizontal patterns divided…
Part Number: DLP4710EVM-LC Tool/software: 我现在用投影仪内部模式投射8bit条纹图案,并同步触发相机拍摄。如图1,每张图的触发上升沿在exposure开始处,而不是pre-exposure处,意味着在投影仪的exposure开始时,相机才开始拍摄。但我看到图2说pre-exposure就会分配给0bit了,但是pre-exposure时相机还没接受到触发信号呢?所以想请教问一下这款投影仪投射图案位深设置为8bit时,其曝光方式是什么样子的,pre-exposure时会分配第0个bit么…
Part Number: DLP4710EVM-LC Hello!
I'm building two projector-camera systems, one infrared, one RGB. The RGB system comprises a DLP4710EVM-LC paired with two DFK 33UX273s, controlled by a Jetson Orin Nano 8GB.
The projector looks fantastic and normally…
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLP4710 , DLP4710LC , DLPC3439 , , DLPC3479 IS DMD 4710LC is different from DMD4710AFQL? I am replacing exiting DMD of DLP4710 with DLP4710AFQL
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLPC3479 , DLPA3005 Hello, I am currently working on a project that requires me to keep only one LED ON, (say the blue LED), while keeping the red and green LEDs turned off. Additionally, I need…