Part Number: DLP4710LC
Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
Please see below.
"Our aim is single-pixel imaging then is it okay if I go with DLP4710LC without the evaluation module? We are not planning for projection…
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLP4710 , , DLPA3005 Hello everyone,
I am developing my DLP4710 projector followed DLP4710EVM-LC.
According to my application, I need a signle bule LED to work. But on the TI.com, there are only…
Part Number: DLP4710LC The Datasheet of DLP4710LC says can support up to -20 degree
I feel it will be only chip set which is non automotive and supports -20 degree, is it a typo or real, Kindly confirm
Part Number: DLP4710 Other Parts Discussed in Thread: DLPC3479 , Hi, I am currently using DLP4710LC and DLPC3479, but availability of DLP4710LC is tight. So is it possible to use DLP4710 (without LC) as an alternative? What are some of the problems that could…
Part Number: DLP4710LC Other Parts Discussed in Thread: DLP4710EVM-LC I have taken DLPC4710-LC EVK for my design
I have generated gerber with the component changes(changed obselete or non available components mostly passives and connectors)
Now i wish…
Part Number: DLP4710LC Other Parts Discussed in Thread: DLP4710EVM-LC , DLPC3479 Hi,
We have Idenfied DLP4710-LC for our requirement
i have went through design files of DLP4710EVM-LC, also procured two nos of kits for evalaution
My video input resolution…
Part Number: DLP4710LC Hi Team,
Our customer made the following inquiry.
Could you tell me about DLP4710LCFQL?
1.Flame retardant grade:5VA>5VB>V-0>V-1>V-2>HB
Answer : Please select 5VA or 5VB or V-0 or V-1 or V-2 or HB
2.Silver migra…
Part Number: DLP4710LC Hello, our team is working on designing optical setup which requires DMD exposed light modulation platform that we could use to develop our optics around it.
we are looking for a small chip and were wondering if 4710 Light control…
Part Number: DLP4710LC Other Parts Discussed in Thread: DLP4710 , Hi,
My customer needs 3D CAD data of the DLP4710LCFQL, they want CAD data that can be used to display dimensional drawings such as the following. Is such data provided? If so, which CAD format…