Hi again
In the end, we bought DLPLCR55EVM_DLP093_REV1. As you have told me for setting up DLPC900 with DLPCR55EVM, we should change the firmware first. So, I have tried to find the DLP5500 firmware to upload it while jumper11 is connected. Unfortunately…
Part Number: DLP5500 Other Parts Discussed in Thread: DLPC200 I am new to using a DMD and coding software for it. I currently have a DLP5500 chipset, and would like to write a matlab or labview code in order to autonomously use it. Is there any material…
Part Number: DLPLCR55EVM Other Parts Discussed in Thread: DLPLCRC900EVM , , DLPC900 , DLP5500 My DLPLCR55EVM board cannot work. When the DLPLCRC900EVM is powered on, D8 and D9 are on while D6 is kept off. I'm sure the DLPLCRC900EVM board and the flexible…
Part Number: DLP5500 Other Parts Discussed in Thread: DLPC200 , , DLPA200 Hello,
I want to display a static image using DLP5500 or any other comparable DMD chip. I want to know if the assicaiated chipset like DLPA200 and DLPC200 is needed for displaying…
Part Number: DLP5500 Hi
I am looking for an explanation of the “hermetic sealing process” used for the DLP5500.
The military standards precludes using organic adhesives to hermetically seal a Microcircuit package.
Obviously , this is not a military device…
Part Number: DLP5500 Is there a Beaglbone cape similar to the DLP Pico that's compatible with the Beaglebone green wireless? If not what would be a viable alternative?
Part Number: DLP5500 Dear all,
I'm currently prototyping a system based on the DLP5500, which for now comes from a Hg-HID lamp-based projector which I "hacked". The ref number of the DLP extracted from the projector is 1076-6439B. Analyzing the reflectance…
Part Number: DLP5500 Hello Everybody,
Is possibloe to solder DLP5500 directly on a thnin PCB (0.8mm) as THT component; i have not found any information about the maximum temperature during soldering.
In case that the compnent isn't solderable where i…
Part Number: DLP5500 Hello,
I heard a document exists which tells users to operate the DMD device with a laser. Can somebody link me to it? Thanks!
Best,
Duc-Quy Nguyen