Part Number: DLP5531Q1EVM Other Parts Discussed in Thread: DLP5531-Q1 Hello,
I have an evaluation board from you, DLP5531Q1EVM, and when I try to display an image, on the DMD, image is wrong, only half is displayed. Also in GUI I have an error: DMD Training…
Other Parts Discussed in Thread: DLP5531-Q1 Hello.
Is the DLP5531-Q1 EVM available?
Can I have any information of DLP5531 chipset? (release schedule, product information etc..)
Best regards, RY
Hello -
Have you programmed the EDID PROM with a binary file? See attached instructions and binary file.
Customer DLPC230 and TPS99000 Fresh PCB Start Up Procedure.docx DLPC230_EVM.bin
The third-part contractor who manufactures and assembles the PCBs of…
Part Number: DLP5531Q1EVM Other Parts Discussed in Thread: DLP5531-Q1
i have DLP5531-Q1 evm and i want to light up the headlight by DLPC230 control program.
i have so many questions
①when i turn on the power,the red light(D8) light up,is that…
Hello Yin -
This page is a post for the DLP5530PGUQ1EVM, which supports HUD applications. For DLP5531-Q1 and headlight applications, please use another E2E thread.
Regards,
Ross
Hi Shuo,
The DLPC230-Q1 typically runs at a video input frame rate of 60Hz. The video latency is one frame, meaning 16.66ms is the time it takes for the DLPC230-Q1 to receive the video data, process it, and display on the DLP5531-Q1 DMD. You can read…
Hi Yongxin,
Yes, the DLP5531-Q1 is used to achieve the showcased performance and currently the only high resolution exterior headlight DLP DMD based chipset available on the market today.
To better answers questions 1, 3, and 4, please use the DLP-OMM…
Part Number: DLPC230-Q1 Other Parts Discussed in Thread: DLP5531-Q1 , DLP5530-Q1 Hi all,
When using DLPC230 Control Program, I could change dimming setting. My question is is there a way to write a simple script (like a python file or batch script file…
Part Number: DLP5530-Q1 Other Parts Discussed in Thread: DLP5534-Q1 , , DLP5531-Q1 Hi DLP Experts, We need your assistance on this as our customer needs more information before choosing their DMD. We have studied the datasheets of DLP5534-Q1, DLP5531-Q1,DLP5530…
Dear Fizix
Thank you for your reply.
1. R/G/B Color
2. Power : The strongest LED brightness
3. Expected measurement distance : over 1~2M , Measurement range : 1M
I think that DLP4710 series EVMs are strongest brightness. What do you think?
What is a difference…