Cherry,
The DLPC230-Q1 has many diagnostic features to ensure that the system is operating safely. Thus, if the input video is not "valid", then it will automatically switch to standby mode. However, it will not automatically switch back to display…
Part Number: DLP5531Q1EVM Other Parts Discussed in Thread: DLP5531LEQ1EVM Tool/software: Code Composer Studio Hi
When I use DLPC230 Control Program Lite 1.8 Build 1242 to read the bin file and program, the error is displayed at the end of the reading…
Part Number: DLPC230-Q1 Other Parts Discussed in Thread: DLP5531Q1EVM , Hi Expert,
Seeking advise on this:
I bought your DLPC230-Q1 chip and want to make a DLP5531Q1EVM board. May I ask if I downloaded its internal program directly from FLASH?
Instead…
Part Number: DLP5531Q1EVM Other Parts Discussed in Thread: DLPC230-Q1
When I use the external video interface of DLP5531Q1EVM, I always get an error indicating that my external clock frequency is out of range. Why does it come out?
Hello Chen,
I don't know what program that is a screenshot of. The DLP5531Q1EVM can display video from an HDMI connection. This is the easiest way to display headlight content on the EVM. The HDMI port is configured to work with any standard HDMI output…
Part Number: DLP5531Q1EVM Other Parts Discussed in Thread: DLP5531-Q1
i have DLP5531-Q1 evm and i want to light up the headlight by DLPC230 control program.
i have so many questions
①when i turn on the power,the red light…
Part Number: DLP5531Q1EVM Other Parts Discussed in Thread: DLP5531LEQ1EVM
Hello,
I came across this video featuring a demo of the DLP headlight, and would like to understand what solution can be used specifically to control the output - if there is…
Part Number: DLP5531Q1EVM Now I can show any preset light type and video through it, but how to realize adaptive lighting?
Is it through the script function of the GUI software shown in the figure? If not, how should this script function be used, because…