Part Number: DLP6500FYE Other Parts Discussed in Thread: DLP6500FLQ
Tool/software:
Hi,
we use DLP6500 to expose 8-bit patterns on photoresist using a 405nm laser.
DLP 6500 works in Video Pattern mode and the laser is controlled by the LED R output…
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLPC900 , DLPLCR65EVM , , DLPLCRC900EVM I'm trying to follow instructions on setting up my DMD and evaluation board on Lightcrafter software. I have the issue that on the operating mode, I can't…
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLPC900 , DLPLCR55EVM , DLP5500 , DLPLCR65EVM Hi,
I own a DLP6500FYE device, which has been functioning correctly for a while. However, it has recently encountered issues. Specifically, I'm…
Part Number: DLP6500FYE Hello, I would like to ask a question. I built a projector system with DLP6500: a laser shoots on the DMD chip with an elevation angle of 24° and an azimuth angle of 45°. The pattern will be projected directly above the DMD chip…
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLP7000 I intend to use a TIR prism I would like to use a DLP6500 or DLP7000, but they must be illuminated from a position perpendicular to the micromirror hinge axis, i.e. 45°, and at an angle…
Part Number: DLP6500FYE Hi,
I am working on a custom application where we are sending messages to the DMD using the USB HID api to load various images. As part of my driver API, I have built in a cyclical status check that occurs in the background to…
Part Number: DLP6500FYE When the output light from the laser diode is collimated and irradiated to the DMD, several images of reflected light from the DMD appear to overlap. What could be the cause of this? I am using a DLP6500FYE Thank you.
Part Number: DLP6500FYE Other Parts Discussed in Thread: DLPC900 Hi,
I purchased a DLP6500 DMD and it doesn't work recently. It worked properly before but suddenly the GUI can't controll the DMD board and the same pattern (shown in the 1st picture…
Part Number: DLP6500FYE Hello Team,
Can you please tell me what is the maximum power that can be used without damaging the modulator? I found this information on the official website: 1) In the visible range up to 25 W/cm2 and thermally limited; 2)…
Part Number: DLP6500FYE Hi Team,
Our customer bought DLPLCR6500EVM in 2018. However, recently someone disassembled the DLP6500FYE from the board and then it doesn't work anymore. I have asked the customer to reseat the flex cable and DLP6500FYE to ensure…