Part Number: DLP650LNIR Other Parts Discussed in Thread: DLPA200 , DLPC410 Hello,
I would like to dynamically shape a continuous-wave laser source (laser diode) at 940 nm with a power of 200 W (with the option to reduce the power if necessary). Initially…
Part Number: DLP650LNIR Hi,
I am using DLP650NIR devices in the optical systems that I am building and I want to figure out the material limits of the device. Currently, the DMD is being illuminated by an ultrafast pulsed laser source and my calculations…
Part Number: DLP650LNIR Other Parts Discussed in Thread: DLPC410 Tool/software: Hi!
I have a couple of question about the following product: DLP650LNIR.
I understand that the refresh rate is 12.5 kHz, however, I read that it only takes a mirror 1…
Part Number: DLP650LNIR We are using a DMD (DLP6500LNIR) illuminated by a 1030 nm femtosecond laser. The incident angle on the DMD is approximately 24°. After reflection from the DMD, the beam passes through a 4f system for beam size reduction (with focal…
Part Number: DLP650LNIR Hi sir/miss,
We need us DLP650LNIR for our product.The datasheet show ou to 160-w incedent on DMD.
May I ask one question?
Our opitical efficient is 49% from laser to illuminatin output(that is beteen DMD and project lens…
Part Number: DLP650LNIR Other Parts Discussed in Thread: DLPC410
Dear TI,
I have a question about DLP refresh rate, particularly the DLP650LNIR. We are using the DLP650LNIR coupled with the controller board from Vialux.
From the datasheet, it is…
Part Number: DLP650LNIR Other Parts Discussed in Thread: DLPLCR65NEVM , DLPLCRC410EVM Dear Sir/ Madam
I just place order online ( order No. T06095091 ) as 3 items : DLP650LNIRFYL , DLPLCR65NEVM and DLPLCRC410EVM
We would like intergarte use it, please…
Part Number: DLP650LNIR Tool/software: Hello,
I am right now working with a DLP650LNIR for my master thesis. Because we want to use the DMD later to influency atoms in a MOT, we want the output to be as stable as possible. I realised, when looking at…
Part Number: DLP650LNIR Other Parts Discussed in Thread: DLP4500NIR , DLPC410 , DLPC350 , DLP4500 Tool/software: 1. What is the difference between DLP650LNIR and DLP4500NIR? Is it just a much higher refresh rate? When would it be justified to have that…