Part Number: DLP7000UV
Hi All,
We have a DLP7000UV DMD. We use a UV source with spectrum 320-500nm. Previously after reflection from DMD we used to get 25mW/cm^2 intensity when measured with 365nm sensor radiometer, but now with the same setting we are…
Part Number: DLP7000UV Other Parts Discussed in Thread: DLP7000 Hi,
I have a question about the refresh rates of DLP7000UV. I understand that it is 32kHz for a single bit. Does it mean that to change all the pixels for a 1024x768 device, it takes about…
Part Number: DLP9500UV Other Parts Discussed in Thread: DLP7000UV , DLP7000 , DLP9500 I am trying to modify an existing 3D printer to use a 365nm projector, and TI's DLP7000UV and DLP9500UV DMDs are the all I can find. I don't I know enough to build…
Hello again Richard,
If the version on the PROM is DISCO3000-004 then a newer DLP7000 or DLP7000UV will work in the system, but will only run at 1xLVDS speed - 100 MHz clock (limited by the controller).
Fizix
Part Number: DLP7000UV Hi Forum,
I´m working on a application for the DMD´s that will enable a camera to look at different regions of the electromagnetic spectrum.
The UV DMD´s are positioned on the UVA part of that spectrum, from 363 to 420…
Other Parts Discussed in Thread: DLP7000 , DLP7000UV , DLP9000 Good morning,
I would know if the component DLP7000 or DLP7000UV is compatible with ‘DMD XGA 825 S1076-9145 42F18Y 050374E’.
I was searching for DMD XGA 825 and I found the most…
Other Parts Discussed in Thread: DLPC410 Hi,
I am working on designing the DLP Application with the DLPC410 chipset for driving the DMD 7000uv and 9500uv.
How can I find the part no. and datasheets of the LGA socket for 7000uv and 9500uv ? Also I need…
Other Parts Discussed in Thread: DLP7000 , DLP7000UV
Hi,
I'm now setting up new illumination system for our DMD set-up (DLP7000 and DLP7000UV).
So, we need reflectance and diffraction efficiency with respect to irradiation wavelength. especially for…
Part Number: DLI-3P-DLI41XX Other Parts Discussed in Thread: DLP9500UV , DLP7000UV , DLP4500 , DLP9000 , DLP7000 , DLP6500FLQ , DLPC900 , DLPC910 Hi,
I would like to know the differences between DLI-3P-DLI41XX and DLPLCRXX00EVM (4500, 6500, 9000). Which one has…
Part Number: DLP7000 Other Parts Discussed in Thread: DLP650LNIR , DLPC410 , DLPLCR65NEVM Has any of the DMDs been released with NIR or NIR2 window?
I see DLP700 and DLP7000UV, for example, but DLP7000NIR is nowhere to find.
Thanks.