Part Number: DLP9000 Other Parts Discussed in Thread: DLPC910 , DLPC900 , DLP7000 , , DLPLCR90EVM , DLPLCRC900DEVM Tool/software: Hi,
Customer needs a full working set to test DLP 9000 which could accept the continuous image stream to display image…
Part Number: DLP9000 Hi, I am new to using DMD. I want it to do structured illumination microscopy. I want to use my DMD to generate a sinusoidal grating that I can rotate and translate. I want the DMD to act like a grating that I can rotate and translate…
Part Number: DLP9000 I have a dual dlp900 controller setup with 2560x1600 resolution. I would like to operate with 66.6666Hz frame rate so that I can have three 5msec patterns on 15msec frame boundaries giving me an effective 200Hz pattern rate.
I have…
Part Number: DLP9000 Tool/software: Hi I am currently using DLP9000 and I am projecting a diffraction grating on the screen and capturing the image using prime BSI express camera. I have to take multiple images with different orientations and doing it…
Part Number: DLP9000 Dear TI,
we are considering the application of a DLP module to create a synthetic "slit" for a scientific prototype.
This expepriment will need to operate well below 365 nm so the protective glass in front of the array is a limitation…
Part Number: DLP9000 Other Parts Discussed in Thread: DLPC900 Hi, I am a newbie for DLP. I am wondering what is the frequency of the mirror flipping in the idle mode. I am using DLPC900 controller and DLP9000 DMD. I couldn't find the relevant information…
Part Number: DLPC900
Hi
Is it posible to Invert the data inputs in a Video mode as in a pattern mode?
We would like to place the DMD9000 in a 180º (new layout) and flip Image Short-Axis , the Front light is in the same location
then we do…
Part Number: DLP9000 Other Parts Discussed in Thread: DLPC900 Tool/software: Hi, I looked through the Python code and realise that the encoded length for the 1-bit images length is different with 8-bit images. ( I am using the same image just different…
Part Number: DLP9000 Other Parts Discussed in Thread: DLPC900 Currently I am following the manual to add images into the flash memory. However, I do not understand what each step is doing. I was hoping to clarify what the below steps are so I can know…
Part Number: DLPC900 I have DLP electronics circa 2015.
How do I find out what Firmware Version is in the board sets?
Has tehere been a firmware update since then?