Charles,
Yes, unless it is a very humid environment the DLP6500FYE will work fine.
That can be a bit misleading. That is across all supported DMDs. For the same resolution (i.e. DLP6500 on DLPC900 vs on DLPC910 the ,DLPC910 can put out binary patterns…
Part Number: DLPC910 Other Parts Discussed in Thread: DLP9000X ,
Hello,
I'm working with DLPC910 and DLP9000x, I'm driving DLPC with Xilinx FPGA (xcku060).
I'm having problems after few hours of work, it seems that the first rows are blank (or float…
Part Number: DLP9000X Other Parts Discussed in Thread: DLP9500 , DLP9000 Hello,
DMD Active array dimensions given in datasheet 19.354 x 12.096 (W x H) ( 7.11 Micromirror Array Physical Caracteristics) from http://www.ti.com/lit/ds/symlink/dlp9000.pdf do not…
Part Number: DLP9000X Other Parts Discussed in Thread: DLPC910 , , DLP9000 Hi,
I have a dlp product-----v-9001 from Vialux,whose chipset is dlp9000x and dlpc910. It is the visible version,so the illumination wave length is 400-700nm,and the damage ilumination…
Part Number: DLP9000
Hi Team,
Can you please help us with our customer's inquiry below.
I am curious about the DLP9000 versus the DLP9000X. The datasheet states that the maximum operating temperature T_array is 40C for the DLP9000X, regardless of…
Other Parts Discussed in Thread: DLP9000X If mating connector for DLP9000X (355 pins) should be Amphenol 8448-001 (335 contacts)? Other 20 pins should not be used for production, am I right?
Other Parts Discussed in Thread: DLP9000X Where can I find footprint (land pattern) recommendations for DLP9000X part?
For example, there is a good technical datasheet for 0.7 XGA, name for this document is 2503870.
Is there the same type of document for…
Part Number: DLP9000X Can we use the FPGA and external circuit designed by ourselvs without the DLPC to operate the DMD, in order to get a higher speed?