Part Number: DLP9000XUV I am working on a DMD kit constructed by ViALUX (V-9001 UV), in which the DMD chip is DLP9000XUV. While I created a grey scale pattern for test (4x4, see below) and displayed it (only one frame, illuminate time = 4s, 8-bit, other…
Part Number: DLP9000XUV
Is it possible to design a DMD to operates with two states: off state and parked (flat) state?
From the answer of other similar questions, I've found that this type of operation has long term reliability issue.
But I think…
Hello Tim,
Are you able to measure (in pixels) the distance from one line artifact to the next one?
This type of artifact is typically the result of a poorly connected or not connected single LVDS line. Please check the Controller and DMD board pads for…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: DLP9000XUV Tool/software: I am looking for DLP lightCrafter product with add-on specifications like DLP 4K resolution and UV-light output.
Hello Hafiz,
The DLP9000X DMD that is run by the DLPC910 controller runs at higher speed (480 MHz) than the DLP9000 DMD.(400 MHz).
If you use 405 nm then you can use the DLP9000 (DLPC900 controller) or DLP9000X (DLPC910 controller)
If you plan to use…
Hello Lorenzo,
I am jumping in here with Michael. Neither the DLP9000 or DLP9000XUV part will reach down to 200 nm. The glass has 0 transmissivity at that wavelength. We do not support removal of the window as there is proprietary material inside the…
Michael
The DLP670S DMD is not rated per the data sheet to operate with 385 nm light. The lowest wavelength it is specified to use is 420 nm.
For an industrial 3D printer utilizing the 385 nm the TI DLP9000XUV https://www.ti.com/product/DLP9000XUV would…
Part Number: DLP9000X Other Parts Discussed in Thread: , DLP9000 , DLPC900 Hi,
We have DMD devices with DLP9000X and DLP9000XUV chips (V-9001 and V-9001UV, ViALUX). When doing the calibration of grayscale, we found that the output power is not proportional…
Part Number: DLP9000X Other Parts Discussed in Thread: , DLPC910 We are looking for DMD setup that enables gray scale output (≥8bits) in UV/Vis wavelength. In my first glance, the DLP9000X/DLP9000XUV chip can meet our requirements. But I am confused with…
Dear Fizix
Thank you for your reply.
1. R/G/B Color
2. Power : The strongest LED brightness
3. Expected measurement distance : over 1~2M , Measurement range : 1M
I think that DLP4710 series EVMs are strongest brightness. What do you think?
What is a difference…