Part Number: DLP9500 I try to use a pulsed laser to illuminate the DMD mirrors (DLP9500) with modulated patterns, and I want to know if DMD can withstand laser with the following parameters: Laser:532nm Pulse energy:3mJ Pulse width:5ns Repetition rate:2k…
Hello again Huang,
The optical team indicates there is not enough information here to make any significant evaluation. They have asked for the following information:
Please share the optical system, wavelength of the laser and f/# and AOI of the illumination…
Part Number: DLP9500 Hello,
We used an V-9501 module from ViALUX to control our DLP9500 DMD. It suddenly got an display issue recently. The left half of the DMD display always showed vertical stripes overlapped with the image regardless of the image we…
Part Number: DLP9500
Hi,
We use the DLP9500 DMD for our product and now there are some failure device when we load the program,
We consider the below reason for the issue and please advise how to improve the technology, thanks.
1. Temperature: Is there…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPLCRC410EVM , DLPLCR95EVM , DLPLCR65EVM , DLPC900 , DLPLCRC900EVM Hello,
I am a postgraduate, I'm hoping to use DMD as a controllable "pinhole array" in a confocal measurement system, as a subsitute…
Part Number: DLP9500 Hi,
I have a customer who uses DLP9500BFLN and found that the MSL is level-NC-NC-NC. What does that mean, please?
How does the customer need to store these devices? Do you have relevant documents that you can explain?
Thank you~ …
Part Number: DLP9500 What is the damage threshold about dlp9500 at 355nm? Is there have any customers application at 355nm ? IF the mean power density is 480 mW/cm² , can the 9500UV nolmal use?
Part Number: DLP9500 Hi,
A while ago I asked about removing the protective window over the mirrors of a DMD. We want to use the DLP9500 since it is the biggest array diagonal size with a mirror size of about 10 microns or less. We intend to use it for…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPLCRC410EVM , , ALP Hello everybody,
we are planning on building a lithography setup using the DLP9500. Unfortunately, we were unable to purchase control boards like the recommended DLPLCRC410EVM due…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPC410 Hello First of all, thank you for your kind reply. I'm asking you an additional question, so please check it out. 1. What is the actual skill level of Data Load Time 5.76 μs/2Block? (Ex)…