Part Number: DLP9500 Other Parts Discussed in Thread: DLP9000 Hi,
I have a design question in regards to the DLP9500BFLN interposer selection matrix document. Following the directions provided in that document, I've selected an interposer TI DWG # …
Part Number: DLP9500 Other Parts Discussed in Thread: DLPC410 , DLPC900 I don't have much experience in developing the DLP device, so I got a few questions.
I want to play thousands of images(1080x1920 BMP) on an endless loop. But I find it very hard…
Part Number: DLPC410 Other Parts Discussed in Thread: DLP9500 , DLPLCRC410EVM , Hello,
According to the datasheet of DLP9500,the max pattern rate is 23418Hz. But DLPLCRC410EVM can not meet the requirment.
So, how can I design to meet the requirment as much…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPC410
we have two DLP9500BFLN DMD can not do projection image ,But we replace new one DMD in same circuit test is normal having projection image..
see the photo and video in attach. PLS help analyse…
Part Number: DLP9500 Hi team,
If the chip of DLP9500 visible band is used in 900nm infrared band, how high is the optical efficiency? This chip has 10.6um pixels and 1920*1080 pixels.
What is the overall optical efficiency of 900nm?
There is only a curve…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPA200 , DLPC410 Hello,
DLP9500 should be used 2 DLPA200s. Reference schematic connects DLPA200 A side to DMD VCC2. Is there something of problem if DLPA200 B side is connected to VCC2 instead of DLPA200…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPA200 Hello,
Each schematics assigns zenner diode as below. However, the comment says both assignment is not correct. Can we remove D8 on DLPA side or D1 on DMD side?
Part Number: DLP9500 Other Parts Discussed in Thread: DLPA200 , Hello,
According to DLPA200 datasheet, TI recommends "Coilcraft DT1608C-223" as an Inductor for VRESET_SWL. However, the parts has already been EOL. Would you please tell me a substitute…
Part Number: DLP9500 Other Parts Discussed in Thread: DLP7000 Dear TI, During exploitation some of the pins at the back of the DLP9500 DMD were broken and were lost (see the attached image). Could you please send 12 pins, thus, we will be able to repair…