Part Number: DLP9500UV Hello,
We are planning on applying the DLP9500UV into a laser system (COMPEX300 - manual attached) to project larger scaled images. However, the wavelength of the current laser system is 351 nm, which is slightly lower than the…
Part Number: DLP9500UV Other Parts Discussed in Thread: DLPC410 The DMD is projecting, however it is only projecting a screen with vertical stripes of black. Wondering how to fix this issue. Tried resetting the board as well as the mirrors. Can't get the…
Part Number: DLP9500UV Other Parts Discussed in Thread: DLPLCR95UVEVM , DLPLCRC410EVM , DLPC410 , Hello,
We are interested in using the DLPLCR95UVEVM + DLPLCRC410EVM bundle for 3D printing applications and would like to know if there are any programming guidance…
Other Parts Discussed in Thread: DLPC410 Hi,
I am working on designing the DLP Application with the DLPC410 chipset for driving the DMD 7000uv and 9500uv.
How can I find the part no. and datasheets of the LGA socket for 7000uv and 9500uv ? Also I need…
Part Number: DLP9000XUV Other Parts Discussed in Thread: DLP9500UV We are now purchasing DMD products that can be used in the 355nm plused laser.
The products DLP9000XUV and DLP9500UV can be used in the band of<400nm, but the maximum illumination power…
Hello User,
Please see page 14 of the DLP9500UV datasheet . The environmental specifications show that the power specification below 365 nm is only 2 mW/cm^2. We do not recommend applications below 365 nm wavelength.
Fizix
Part Number: DLPLCRC410EVM Other Parts Discussed in Thread: DLP9500UV , , DLPLCR95UVEVM , DLPC410
Hi, I have the assembly of DLPLCR95UVEVM and DLPLCRC410EVM. I want to connect to DLPLCRC410EVM and load images on DLP9500UV using Python. Is that possible…
Hi Dominic,
we would be happy to help you with our DLP9500UV based setup ( www.vialux.de/.../superspeed-specification.html) including the proven ALP Controller Suite. Also, thanks to our compact form factor, you can set up multiple boards side by side…
Moshe,
As a point of clarification, this is the same DMD that was previously being used so that the DMD_TYPE is the same. If I read your post correctly this is the DLP9500UV.
I am sending a private message regarding this since I know that some of the…
Part Number: DLI-3P-DLI41XX Other Parts Discussed in Thread: DLP9500UV , DLP7000UV , DLP4500 , DLP9000 , DLP7000 , DLP6500FLQ , DLPC900 , DLPC910 Hi,
I would like to know the differences between DLI-3P-DLI41XX and DLPLCRXX00EVM (4500, 6500, 9000). Which one has…