Part Number: DLPA200 Other Parts Discussed in Thread: DLP7000UV , DLPC410 , DLPLCRC410EVM Tool/software: Dear Texas Instruments Support,
I am an engineer developing optical equipment using DLP technology.
Over the years, I have developed numerous…
Part Number: DLPA200 Other Parts Discussed in Thread: DLPC410 , DLP7000 Tool/software: I have designed a custom PCB using the DLP system (DLPC410, DLPA200, DLPR410, DLP7000). In my design, the DLPA200 is not providing the VBIAS, VRESET or VOFFSET voltages…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPLCR95EVM , DLPLCRC410EVM , DLPA200 , I buy DLPLCR95EVM +DLPLCRC410EVM , before power on, I have some questions
The user's guide “DLPU040A DLP ® Discovery 4100 Development Platform User's Guide…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPLCR95EVM , DLPLCRC410EVM I buy DLPLCR95EVM +DLPLCRC410EVM ,
1. The U5 and U11 is very hot. Do I need a heat sink ?
2. The heat sink of the DLPLCR95EVM is very hot . Need additional heat sink…
Part Number: DLPA200 Hi E2E support,
I'm sorry for delayed response.
My customer is looking for a Zener Diode meets the Hardware Specification.
Would you please tell me about TI recommended device?
Best Regards,
Koike
Part Number: DLPA200 Other Parts Discussed in Thread: DLPLCRC410EVM Hi E2E support,
According to DLPA200 datasheet, a value of VOFFSET/VCC2 filter capacitor is 1-4.7 µ F.
Note : Recommended value is 3.3 µ F each.
Different values are acceptable…
Part Number: DLPA200 Hello,
D1 Zener diode tries to clamp VCC2 driven by DLPA200's Voffset in appropriate voltage range BZD27C8V2P has following tolerance between 7.7 V to 8.7 V. If the tolerance goes min, the VCC2 becomes less than 8.25V. So, would…
Part Number: DLP9500 Other Parts Discussed in Thread: DLPA200 , DLPC410 Hello,
DLP9500 should be used 2 DLPA200s. Reference schematic connects DLPA200 A side to DMD VCC2. Is there something of problem if DLPA200 B side is connected to VCC2 instead of…
Part Number: DLPA200 Hi, Good day. Our customer is looking for an equivalent part for DAD1000. With this, can they use the DLPA200? Is this a drop-in replacement for it? If no, we would appreciate if you could suggest a device that they could use. Thank…
Part Number: DLPA200 Hello,
In our product we use DLP chipset to drive a DMD.
For testing the board used to drive the DMD , we use JTAG.
So, via JTAG we can control the DLPC and DLPR chips with one exception , the DLPA chip has no JTAG access. …