Part Number: DLPA200 Hello,
In our product we use DLP chipset to drive a DMD.
For testing the board used to drive the DMD , we use JTAG.
So, via JTAG we can control the DLPC and DLPR chips with one exception , the DLPA chip has no JTAG access. …
Part Number: DLPA200 We have had a recent rash of DAD2000 Voltage Boost Converter Circuit Capacitor failures, specifically the VBIAS and VRESET filter capacitor, specified to be 1 to 10uF, 35V, 1 Ohm ESR. We are using Vishay TR3C335K050C1500 – 3.3uF 50V…
Part Number: DLPA200 Hi,
I can not find the DLPA 200 PFC.
Is DLPA 200PFP the successor product? Is there compatibility?
I would be pleased if you give me advice.
Best Regards,
Leonardo
Hi Florian,
Welcome to the E2E forum! I apologize for the delay in response!
1) The power consumption for the DLP7000 is not provided because it can vary quite a bit depending on your use-case, much like our other chips (more on this later).
2…
Hi Trevor
Thank you for your reply
Please help me to understand what steps you have taken to troubleshoot this problem so far, have you tried replacing the DLPA200 ?
=> Yes, I tried to replace the new DLPA200 chip.
As a result, my board is normal…
Other Parts Discussed in Thread: DLPA200
Hi,
There are unclear specifications on datasheet "DLPA200.pdf DLPS015A". Could you clearfy specifications below?
-DC specification of VBIAS(absolute Maximum Rating, recommended operating range)…
Part Number: DLP7000 Other Parts Discussed in Thread: DLPA200 , DLPC410 Tool/software: I have a few questions regarding the mirror clock pulses (MCP) that are sent to update the physical state of mirrors in each block for the DLP7000. When I measure the…
Part Number: DLP650LNIR Other Parts Discussed in Thread: DLPA200 , DLPC410 , DLPC350 , DLP4500NIR Tool/software: What are the lead times for ordering the:
DLP650LNIR and DLPC410 and DLPA200.
DLP4500NIR and DLPC350 and DLPA200.
I see that the…
Part Number: DLPC410 Other Parts Discussed in Thread: DLP9500 , DLPA200 , , DLPR410B Hello. In the last project, I designed based on DLP9500 reference boards such as DLPC410, DLP9500, DLPR410A, and DLPA200. There were some problems, but it worked well…