Part Number: DLP9000 Other Parts Discussed in Thread: DLPLCR90EVM , DLPA200 Hi,
I am currently working with the DLPLCR90EVM. The intro to 12 deg Digital Micromirror devices guide talks about a mirror clocking pulse that changes the mirror according…
Hello again James,
Rather than recreate the answers in this thread, please look at the following thread:
https://e2e.ti.com/support/dlp/f/94/p/935255/3472192?tisearch=e2e-sitesearch&keymatch=DLPA200#3472192
This should answer the questions you have…
William,
I doubt whether you will be able get down to the level you want. Even if you were able to suspend the APPS_FPGA power draw completely.
The DLPC410 FPGA (Virtex 5 LX30), one of the DLPA200s, and the DMD still have to run. The DMD alone generates…
Hello user,
Are you wanting the power for the full chipset or just the DMD?
The chipset requires a controller (DLPC410 and an analog driver (DLPA200) along with the DMD.
For our kits we recommend a 5V 6A supply.
FIzix
Hello Uryyy,
I am not sure I understand your question. The situation that you describe is the only way that the DLPC410 communicates with the DMD. The DLP9500 SCPDO to DLPC410 SCPDI is required. This is how the DMD ID is read by the DLPC410 controller…
Hello Raphaël,
Thank you for the images and the drawing. Please allow me a day to study this, as I am not sure at the moment what might be going on.
Can you measure the rail voltages on the DLPA200? The only thing I can think of is that the Bias Voltage…
Enid,
You can use the DLPA200 data sheet for pinout. There are only three pins that were different - 51, 52, & 54.
On the DLPA200 they are NC (no connect), but on the DAD1000 they were 51 & 52 were 12V_SWL and 54 was VCC. You should not need to…
Part Number: DLP5500 Other Parts Discussed in Thread: DLPC200 , , DLPA200 I have a customer using the DLP5500, DLPC200, DLPA200 on a PCB for 3D image detection.
This product was launched already, but they are seeing returns due to strange patterns in…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLP3010 , DLPA2000 , , DLPA200 Hi
We are working with a custom board with DLPC3433, DLPA2000 and DLP3010.
It can display a splash screen now. The next step is to input DSI signals directly from…