Part Number: DLPA2005 Other Parts Discussed in Thread: DLPC3470 Hello TI experts,
My customer designed DLPA2005 and DLPC3470 for their product, recently they found a problem in their solution.
the problem is, RGB operation is different between the IC…
Hello Anas,
It is reference design for Spectroscopy scanning application. Please use this reference design.
In this application, there should not be any LED load. VLED feature is mainly for projection application where you are driving LED from DLPA2005…
Part Number: DLPA2005 Other Parts Discussed in Thread: DLPC3478 DLPA2005 is operated in the R, G, B of an LED are sequentially.
(Chipset : DLPC3478)
However, I need the condition that the LED can be operated simultaneously with G & B or R & B…
Part Number: DLPC1438 Other Parts Discussed in Thread: DLPA2005 , , DLP300S Hello,
I'm trying to make sense of the DLPC1438 way of controlling the light which uses dark frames and exposure frames and in general of the DLPC1438 + DLP300S + DLPA2005 combination…
Part Number: DLPC3470 Other Parts Discussed in Thread: DLPA2005 , , DLP2010LC
Hello,
I was currently conducting a development test using DLPA2005 + DLPC3470 + DLP2010LC.
that was design for the Powerup sequence provided by DLPC3470 datasheet, but DLPC3470 Chip cannot…
Part Number: DLPA2005 Other Parts Discussed in Thread: DLPC150 , DLP2010NIR Hi,
I am interested in programming DLPA2005 using its SPI port. In the reference design the pins are connected to DLPC150 PMIC SPI pins. In the datasheets its said that DLPA2005…
Part Number: DLPA2005 Team,
I was looking over the DLPA2005 datasheet and it seems that the input current on VIN should be a typical of 15mA (In active mode with motor excluded). I had a few questions in regard to this…
What is the maximum input…
Part Number: DLPA2005 Other Parts Discussed in Thread: DLPC3435 , DLP2010 I am using DLPA2005, your company product.
The value of LED_SEL [1: 0] is abnormal during use. The clock of SW4 ~ SW6 should be generated by the circulating circuit, but it is fixed…
Part Number: DLPA2005 Other Parts Discussed in Thread: DLPC3435 1. We make and use our own hardware, and we use DLPA2005 and DLPC3435. 2. When designing on its own, I referred to the Datasheet provided by TI. 3. The firmware was also used by our company…
Part Number: DLPA2005 Other Parts Discussed in Thread: DLPC3478 Hi,
today I came across strange issue. DLPA2005 is used as a PMIC for DLPC3478. When PROJ_ON is pulled low, the 1V8_DLPC on LS_OUT falls just to 0V95 while I would expect 0V as the other…