Part Number: DLPA3000 Other Parts Discussed in Thread: DLPC3478 Tool/software: Hello,
I’ve successfully developed my project base the following platform:
Hardware is DLPC3478+DLPA3000;
Firmware is modified based the original version generated…
Part Number: DLPC3432 Tool/software: Dear TI engineer,
I found that the DLPC3432 power off sequence was abnormal when i tested the waveform.The specifications require RESETZ to power off the controller first, and then power off the controller.
But…
Part Number: DLPC3432 Other Parts Discussed in Thread: USB2ANY Tool/software: Dear TI engineer,
Our projection occasionally appears the problem of flower screen and stuck in the first frame, help to see how to analyze this problem,tks!
Part Number: DLPA3000 Other Parts Discussed in Thread: DLP4710LC , DLPC3479 hello TI experts:
after DLPA3000 auto-initializing, HOST_IRQ is low, INT_Z generates one pulse(I think it is not a fault), then DMD HV Voffset Vrst is low,
Q1: is it normal…
Part Number: DLPA3000 Other Parts Discussed in Thread: DLPC3478 ,
Hi, we have a custom made board with DLPA3000 and DLPC3478. We have some issues with power output of dlpa3000.
As stated in power up sequence of DLPA 3000 , we have power until PWR1…
Part Number: DLPC3432 Other Parts Discussed in Thread: DLPA3000 , , DLP230GP Tool/software: Dear TI engineer:
Our company is using DLPC3432+DLPA3000, the DMD can not be lit, the test found that DMD_DEN_ARSTZ has no waveform, but the motherboard has…
Part Number: DLPA3000 This is a question regarding the startup sequence of DLPA3000.
The startup timing of SYSPWR and PROJ_ON is 5ms or more (>5ms), but there are some samples that will not work if this timing is just barely 5ms. The actual value of…
Part Number: DLPC3479 Other Parts Discussed in Thread: DLP4710LC , , DLPA3000 , DLP3010EVM-LC
My hardware combination is DLPC3479+DLPA3000+DLP4710LC.
During the power-on process, dlpc3479 did not send commands to dlpa3000 through spi, which may have…
Part Number: DLPA3005 Other Parts Discussed in Thread: DLP3010 , DLPC3438 , DLPA3000 , , DLPDLCR3010EVM-G2 Hello,
I have a driver board( dlpa3000+dlpc3438+dlp3010, 280lm), now I want to make the dlp much higher( maybe 25% higher other than 100% higher…
Part Number: DLPA3000 Other Parts Discussed in Thread: DLP3010 , DLPC3478 , Dear Sir:
Experimental environment:
1.DLP3010+DLPA3000+DLPC3478
2. DLPA3000 burned down, LED_ANOD and ground short circuit after power input
3. When only connected with…