Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLP3010 , DLPC3478 , DLPA3000 I have custom board with following two configurations:
(1) DLPC3478 and DLPA3000 and DLP3010
(2) DLPC3478 and DLPA3000 and DLP3010 -LC
And I need firmwares for these…
Part Number: DLPA3000 Dear:
I checked DLPA3000 operation temperature is from 0 degree to 120 degrees, but my application maybe work at -20 degrees, can you help me promote suitable part number can meet the case?
Part Number: DLPA3000 Hi Team,
a customer is working on a surface inspection application. The cameras used to record the projected image have very high frame rates.
The classic RGB sequence causes issues there, because of the rolling shutter of the cameras…
I understand, thank you.
I havn't seen a reference design for an application with the DLPA3000 and DLPC3478. That's why I asked for a possibility to review the schematic on the relationship between these ICs.
Part Number: DLPA3000 Tool/software: WEBENCH® Design Tools hello,TI:
I Have two chip DLPA3000,one chip's silkscreen is 89C3GJTG4 from Digi-Key ,other one is 73AS1JTG4. this chip's silkscreen have different?
Part Number: DLPA3000 Hello,
The RLIM_1 and RLIM_2 are separated internally but is it the same for RLIM_K_1 / RLIM_K_2 and RLIM_BOT_K_1 / RLIM_BOT_K_2 ?
Can two different resistors be used to separate the "R MOSFET" channel from the "P MOSFET" channel…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLP3010 , , DLPA2005 , DLPA3000 , DLPDLCR3010EVM-G2 , DLP3010EVM-LC Hello,
We evaluated a structured light projector base on the DLP3010 EVM (DLP3010 + DLPC3478 + DLPA2005).
It works fine but the DLPA2005…
Hello Christopher,
Sorry for the delayed response but I discussed internally and have the following debug advice.
My suggestion would be to check power rails and signals throughout the path of communication to ensure all chips are powered up and see if…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLPA3000 , Hello Ti experts, I have custom board with DLPC3478 and DLPA3000. I send commands to DLPC3478 to update internal pattern table via stm32. After i call project pattern (9Eh), it does not project…