Part Number: DLPA3000 Other Parts Discussed in Thread: DLPC3435 Dears !
DLPA3000 high rate of defective, about 0.5%. our SCH is the same as TI reference , How can we improve this issue? Thanks a lot !
Part Number: DLP2010EVM-LC Dear everyone
I know that dlp2010evm-lc firmware is designed for DLPC3470+DLPA2005 program. If I change the PMIC, that is, from DLPC2005 to DLPC3000, How can I get the fromware for my solution I can post the schematic for you…
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLP3010 , DLPC3478 , DLPA2005 , DLPA3000 , Since TI's EVM is not strong enough for DLP3010+DLPC3478+DLPA2005, I want to change the LED driver chip to DLPA3000 to achieve a larger light intensity.…
Part Number: DLPA3000 Other Parts Discussed in Thread: DLPC3435 , , DLP2010
Dear all,
We used DLPA3000+DLPC3435+ anhua H15 optical machine
There are some problems now, please help to check
1. In the case of no optical connection, supply power to DLPA3000…
Part Number: DLPC3478 Other Parts Discussed in Thread: DLPA3000 , Dear TI DLP Team
I have a favor to ask you.
We would like to develop DLPC3478 and DLPA3000 and need firmware for this system.
I heard that TI can provide firmware for this chip set individually…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC3478 , DLPA3000 , DLPC3438 , DLPDLCR3010EVM-G2 Hi
I have DLPC3478 and DLPA3000, DLP3010
I see that DLPA3000 can work with DLPC3478 and DLP3010.
So, I tried to use DLP3010EVM firmware with that combination…
Hello LP,
The DLP4710LC EVM would be the brightest EVM. This EVM is based on DLPC3479 controller and DLP4710LC DMD. The DLP4710LC DMD has 1920x1080 resolution. Please refer to DLP3479 datasheet for details on features and capability.
LP Kim said: What…
Part Number: DLPC3470 Other Parts Discussed in Thread: DLPA3000 , DLP2010 Hello everyone
I prototyped the board using the following parts. Controller: DLPC3470 Driver: DLPA3000
The controller farm of DLPC uses the firmware "dlp2010evm-lc_7.3.1.img" of DLP2010…
Part Number: DLP3010 Other Parts Discussed in Thread: DLPA3000 , DLPA2005 , DLPC3478 , Hi,
Let me talk about DLPC3478- DLPA3000 for DLP3010-LC.
In this case, Do you have any reference designs ? I can not see in TI HP.
and DLPA2005 is set register via SPI by…
Part Number: DLPC3438 Other Parts Discussed in Thread: DLPA3000 , Hi, Sir
Currently, we want to know how to defined factory tests, for DLPC3438+DLPA3000.
Which signal need to be test in factory?
Thanks
zhang