Hello Archie,
I assume that your application requires 1-bit patterns at 1000 Hz frame rate. All of products / EVM from Advanced Light Control (High Speed Visible) portfolio can support this requirement.
https://www.ti.com/dlp-chip/advanced-light-control…
Part Number: DLP3010EVM-LC Hi,
We are looking for a sample program to flash the DLP3010EVM via SPI which is equivalent to the feature of the GUI program.
We were able to find the I2C sample programs (e.g. DLPC API), but we can not find the SPI example…
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLPC-API , DLP3010LC Dear Concerned
I've got a DLP3010EVM a week ago, and I test DLPC-API in linux to control internal pattern for my own purpose.
In sample example code in DLPC-API has some…
Hello Taylor,
Can you try to see the behavior with https://www.ti.com/tool/DLPC-API without any modifications and compare that with your implementation?
Regards,
Mayank
Hi Austin-san,
I'm sorry, I was a little wordy.
I am concerned about the LED breaking while the light is on in light control mode,
and I wish I could have detected that in the DLPC-API status, but I found I could not do that this time.
So I was…
Renan,
What chipset configuration or system are you using? Are you using the DLPC150 (nirScan Nano) or are you using a configuration with the DLPC3470 (which supports both the DLP2010LC and the DLP2010NIR platforms).
If you are on the DLPC150/nirScan…
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLPC3479 , DLPC-API I am working with a DPM-E4750-LC. I have been able to compile and to work with the dlpc3479 examples of the DLPC-API-1.10, which is based on the x32 version of the CyUSBSerial…
Hello User,
These questions depend on how you want to design your custom board. TI provides the reference design ( TIDA-080003 ) for DLP3010EVM-LC . Please see the answers below for reference:
1. DLPU074A – section 3: For DLP3010EVM-LC, you need to…
Mayank Khandelwal said:
Just to the let you know - The EVM can also be controlled using an API if you do not want to use the GUI. Kindly refer to the following link for more information regarding the API - https://www.ti.com/tool/DLPC-API
Thanks…
Hello Taylor,
Using Cypress SDK to control and communicate with EVM will be fastest and convenient way. You can also leverage the DLPC API by porting it to Linux.
regards,
Vivek