Part Number: DLPC200 Dear All
Thank you for your support every time.
I referred a thread below and I understood "there is no restriction on repeating the patterns in the DLP_RegIO_WriteImageOrderLut()."
e2e.ti.com/.../574290
My question;…
Part Number: DLPC200 Dear TI Team,
I recently purchased a CEL5500 from DLi and I am working on integrating it with our system via Matlab. Currently I am having issues with the DLL file to link to Matlab. I am getting the following error from the files…
Part Number: DLPC200 Hi,
I have question about SPI Flash requirement. TI recommends M25P64 and W25X64, however I'd like to use other flash device. If it can satisfy the timing requirements below, can I use other Flash device? If you have any concerns…
Part Number: DLPC200
Hello,
I have seen IBIS model of DLPC200. a) It seems that MEM_ODT(AH12) pin uses 50ohm output buffer. So I thinks actual ODT buffer value is 50ohm. Is my understanding right?
b) Do you have possibly to be changed this value…
Part Number: DLPC200 Other Parts Discussed in Thread: DLP5500 ,
Dear,
I've made application board using DLPC200 and DLP5500.
working is good so far but some question as below picture is screen shot in LVDS Clock of DLP5500 board. but duty cycle is…
Watanbe-san,
I am sorry for the delay on this one. I have been working with the SPI interface. There is one signal that is not part of the SPI protocol that is used on the DLPC200 implementation. It is "SLAVE_BUSY". This signal must be monitored to…
Part Number: DLPC200 Dear All,
Thank you for your support.
In order to check defect of display image, we would like to compare image buffer of loaded DDR2 actual memory contents and display image(or flash image data). Is there any way to readback…
Hi,
1. You can ask your customer to compare the speed grade and other timing details matching to the recommended part; if it matches then it will work. Alternatively you can work with the SDRAM vendor about can this be drop in replacement.
2. No …