Part Number: DLPC200 Hello.
I have a question about DownloadBPPfromFlashToExtMem(0x0030) command of DLPC200.
When I send the command via SPI, the expected image does not display. Do you have any advice to display image appropriately via SPI?
Case…
Dear All,
Thank you for your support!
Would you please let me know how to calculate the CRC16 for the supplied data?
There seems to be some ways of the CRC16 calculation in general.
Thank you and best regards,
Rossinag
#1.
YES* It is possible provided the LED driver connected to DLPC200 is fast enough to respond to LED_EN (on/off) signals. On DLPC200 the greyscale values are created by accounting both DMD modulation AND LED modulation. Therefore it is very important…
Sanjeev,
I have tried to cross-reference your point #3 to the LightCommander schematic. I do not see any 2 second timing and everything controlling the global reset signal is hardware circuits. In the LightCommander, 1.2V, 1.8V, 2.5V, 3.3V, and 12V…
Hello,
I would like to know whether we can use products other than TI recommeded as follows.
Are there any actual usage products other than TI recommeded, please let me know.
TI recommeded We want to use
JS28F00AP30BF S29GL01GS
CY7C1011DV33…
Hello Seishin,
I have to consult the hardware team on this.
We highly recommend using JS28F00AP30BF part as described in DLPC200 datasheet. Using any other flash device we don't guarantee the operation.
Regards,
Sanjeev
Dear Sanjeev san,
Thank you for your answer.
I have another question in regard to DLPC200 yet, so please allow me to post in another title.
With My Best Regards
Other Parts Discussed in Thread: DLPC200 I'm experiencing some problems triggering the DLPC200 that I'm hoping someone can help with.
First a brief background on our setup. I'm using this system in Structured Light mode. Our setup is loading 120 images…
Hello Hamada-san,
I got response for the below queries -
>> When it is operating, is DLPC200 controlling so that the interior ODT may be used?
Internal ODT is not used in DLPC200.
>> When the interior ODT is used, is a terminating resistance…