Part Number: DLPC300 I want to use the lightcrafter to project a large number of 24-bits patterns,so I should choose xternal streaming pattern sequence mode to achieve the goal.But how do you get the image to the projector? Is there any sample code? thx…
Part Number: DLPC300 Hi to whom it may concern,
Ask about RESET signal of DLPC300.
Our customer make the RESET from the DMD PWR EN of DLPC300.
Could you please c'k the attached file?
If is there some problem,could you please give any advise?
Best…
Part Number: DLPC300 Hello,
In Win 7, the TCP-IP settings for the DLCP300 are set to be
You can test these to see they are set OK:
But in order to communicate with it, in the GUI (V5.0), we have to set the IP as 192.168.1.98, which is not correct since…
Part Number: DLPC300
A quick question about how the DLPC300 interprets a video frame in extended pattern sequence mode external streaming pattern sequence mode. I want to run only a single RGB channel with 1 bit per pixel to get to the 1440 Hz pattern…
Part Number: DLPC300 Hi,
When I try to connect to the DLPC300 from my computer using a USB connection with the DLP Lightcrafter software,
I am getting an error message and not able to connect. The device is being recognized by the computer.
This is what…
Part Number: DLPC300 Other Parts Discussed in Thread: DLP2010 , , DLPDLCR2000EVM I would like to use DLP pico projectors (Lightcrafter would be OK) in which vibrations are not acceptable. Thus, however quiet, fans are not an option. Is there are water-cooling…
Part Number: DLPC300 In my computer, when connected DLPC300 automatically loads RNDIS driver by Acer (V1.0.0, 1/13/2010), But since my Win OS is 7 (pro), I can also load MS version of this driver (V 6.1.7600.16385, 6/21/2006). Which one should I use? It…
Other Parts Discussed in Thread: DLPC300 Hi Kyle,
One more question:
I found that we can use the solution to save the configuration (store pattern sequence) and the image into the lightcrafter, then set the solution as default. This able to solve the…