Part Number: DLPC3433 Other Parts Discussed in Thread: DLP3010 , DLPA2000 , USB2ANY Tool/software: Hello,
We're experiencing a problem with the DLPC3433 getting stuck on the splash screen during power on when the temperature is higher, but still within…
Part Number: DLPC3433 Tool/software: Hi,
We'll be using this part for our product DLPC3433CZVB, I'd like to make sure that I download the correct firmware for this. For firmware selection, the choices are DLPC3433 or DLPC3433_AR, which one should…
Part Number: DLPC3433 Tool/software: can there be i2c communication on the i2c bus before host_irq goes low? For example: Can the master start sending messages to the DLPC3433, before host_irq is low, and waiting for an acknowledgment transaction vs…
Part Number: DLPC3433 Tool/software: This is in part a follow-up to DLPC3433: Clarifying MIPI DSI input requirements , which has been locked.
We've successfully gotten the DLPC3433 to display a test pattern that we're sending through its MIPI DSI interface…
Part Number: DLPC3433 Hi~ 1. if DMD_LS_CLK(120MHz)'s harmonic over FCC/CE's radiated emission limit value, any suggestion for this problem? 2. can i replace 43 ohm resistor to bead to reduce EMI problem?
Part Number: DLPC3433
Tool/software:
I have the following image of DLPC3433 operation from TI which states that the data lanes enter LP11 state once per frame (which indicates vertical blanking). In the waveform, the data lane signals appear to be switching…
Other Parts Discussed in Thread: DLPC3433 Tool/software: I wanted to clarify the meaning of this line in section 7.3.1.4 of DLPS035E:
"LP mode is required during vertical blanking and vertical sync."
Does this mean that the vertical and horizontal…
Part Number: DLPC3433 Tool/software: We also wish to adjust the RGB timing duty cycles. In our case we would like to increase the Green duty cycle as much as possible to achieve greater brightness in green. This is a green monochrome setup so setting…