Part Number: DLPC3433 Hi,
Anyone interested to know or using DLPC3433 Linux driver, please let me know asap. I'm planning to send DLPC3433 driver to upstream Linux as DSI to DMD DRM bridge. I've already sent v1 before. now Planning to send fixed version…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLP3010 We are trying to design a system that uses a DLPC3433CZVB, DLPA2005ERSLT, and DLP3010.
In order to set the thing up, we had to download firmware from TI.
There appears to be no ability to custo…
Part Number: DLPC3433
I am using DLPC3433 with these firmware settings:
After trying to communicate unsuccessfully with the address 0x36, I ran i2cdetect and found that the address for the DLPC3433 is 0x1B.
Why?
Part Number: DLPC3433 Other Parts Discussed in Thread: TIDA-080003 , DLP3010 In DLPC3433 Datasheet (Rev E) section 10.1 it mentions criteria for selecting a ferrite bead
I noticed in the DLP3010 reference design (tida-080003_dlp3010evm_LC_displayboard_revB…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPA2000 , DLPA3005 , DLPA2005 , DLPA3000
Hi,
I'm having a strange issue while handling the power-on sequence in the Linux driver for DLPC3433.
My design has GPIO's for PROJ_ON, PARKZ, and regulators…
Hello Morgan,
Thank you for providing the part numbers. These two DMDs, although similar, are meant for two distinct platforms. The DLP3010 is designed to be used with a DLPC3433/3438 controller for display applications. The DLP3010LC is meant to be used…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLP3010 Hi,
I'm running Linux-5.13 on DLPC3433 with 720p DMD resolution timings. I did see the image color change in non working condition (like Purple Penguins) and working condition seems to be…
Part Number: DLPC3433 Hi,
6.15 DSI Host Timing Requirements mentioned the range of HS Clock from 85 to 235MHz and the desired value would need to write it on Write DSI HS Clock (BDh) register.
Pixel Clock is the Panel or DMD side clock which is very much…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPA3000 Hello,
How can I create a custom firmware file for the DLPC3433?
I would like to adjust some of the battery management settings, splash screens, and maybe some other settings as well.
Is…