Part Number: DLPC3433 My team is having a hard time routing the MIPI data lines (from DisplayPort to DLPC) on one plane.
In order to match p/n lengths, we can get it down to 2 vias but not less.
Will this suffice or will 2 vias on a line cause too much…
Part Number: DLPC3433 Hello,
What would a proper initialization sequence for the DLPC3433 look like for the I2C commands to send the DLPC3433?
Would something like the following look proper? Am I missing something? We could really use some help!
I2C_BUS…
Jagan,
I am glad to hear that your DSI feed is projecting properly.
In another E2E thread , Philippe and I mention that the DLPC3433 does not support 32-bit formats. The DLPC3433 will, however, support RGB888 (a 24-bit format). I had suggested trying to…
HI:
Our device used QC MSM8953. The DSI mipi support up to 1.5Gbps per lane high-speed mode bandwidth.
But in DLPC3433 spec, mipi dsi only support up to 470Mbps lane speed.so I want to confirm whether 2-lane mipi can support the 720P screen?
Part Number: DLPC3433 Hello, I am trying to follow the DSI guidelines to calibrate my DSI timings. Specifically, I would like to understand the clock requirements for Qualcomm. The guide says that the Qualcomm clock should be double as the TI's clock…
Part Number: DLPC3433 What is the recommended trace width and via size for DLPC3433 to escape the BGA? We will be using the 176 pin package and a board thickness between 62 and 93 mils. Would you advise using microvias? Thanks
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPA3000 Hi,
This is the extension of previous issue, where the actual issue is mentioned on this thread.
I can see some last right horizontal area part is moved to the first horizontal area with…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPA3000 Hi,
I have a board with DLPA3000 and DLPC3433 connected to a light engine (projector module).
I have seen some artifacts in the display image and I am wondering what the cause may be.
Please…
Part Number: DLPC3433 Hi,
I have a custom board with DLPC3433. So far, I am adjusting color tint and brightness levels with RGB LED Current Register 0x54 in order to set the proper white point and brightness levels.
Is this the best way? Or are there…
Part Number: DLPC3433 Dears
We found that when DLP was working, there would be a lot of burrs ,about 1A peak current , when testing the total power consumption. We are quite sure that it was caused by DLP. We tested the development board and had the same…