Part Number: DLPC3433 Hi,
I have the default DSI timings from DLPC3433 DSI for 854x480 resolution with PClk value of 25.9054 MHz. Where did this value documented? I couldn't find it even on DLPC3433 I looking to create DSI timings for 1280x720 resolutions…
Part Number: DLPC3433
Hi,
I am routing the High speed signals of the DLPC3433, and trying to follow the layout the recommendations of the datasheet and reference design as much as possible. However, it has been difficult to find a manufacturer capable…
Other Parts Discussed in Thread: DLPC3433 Hi,
I'm following "DSI Setup and Debugging Guide v1.0.pdf" for setting up DSI routing on DLPC3433 chip.
1. Why PClk is 25.9054 MHz in Example DSI Configuration and Timings? I'm trying to use 720p …
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPC-API Hi,
I'm trying to enable DSI routing for DLPC3433 chip by selecting double buffer mode for 1280x720 with 235MHz clock. Here is the listed sequence.
Projector ON GPIO enabled
Reset Pull…
Part Number: DLPC3433 Hi,
I had the RGB LED Current working once, but it does not seem to be working again. I can set the current to zero with no problems,
i2cset -y ${I2C_BUS} ${I2C_ADDR} 0x54 0x00 0x00 0x00 0x00 0x00 0x00 i
and after that when I read…
Hello Chris,
The out of DLC343X is data to drive DMD which includes controller signal and mirror switching information. The DLPC3433 controller take a video stream and converts in to series of bit plane to create an image through DMD.
Hope this explains…
Part Number: DLPC3433 Is there available any specific design guide to make the escape routes of the DLPC 3433 in a PCB? or may I use a standard fanout for those chip size?
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPA3000 Hello,
I have a DLPC3433, DLPA3000 and a light engine that supports 1280x720 resolution.
I am trying to get it to work with DSI signal from an R16. Along the way, I am trying to set the…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPA2000 , Hi,
I need the firmware for the chips dlpc3433 and dlpa2000 for both i2c addresses. from I see i can get them. However all the binaries for both i2c addresses are identical. Should not they…
Part Number: DLPC3433 Other Parts Discussed in Thread: DLPA3000 Hello,
I am having trouble getting my custom board to boot. The board uses the DLPC3433 and DLPA3000, the scenario is as follows:
1.) I have the optical module (light engine) connected with…