Part Number: DLPC3438 Other Parts Discussed in Thread: DLPA3000 , DLP3010 Hi,
We have develop a board based on DLPA3000 + DLPC3438.
We cannot communicate with i2c bus of DLPC3438.
Power supplies are ok.
DLPC start correctly (HOST_IRQ goes high then goes…
Part Number: DLPC3438 Other Parts Discussed in Thread: DLPA2000 , Hello:
Board info : dlpc3438+dlpa2000+dmd
Use the specified read command, i get the Controller-Device-ID is 0x05 , DMD-Device-ID is 0x60 0x0D 0x00 0x87 .
This system already works, the…
Part Number: DLPC3438 Tool/software: Code Composer Studio Hello TI Expert,
I would like to ask a few questions about the test pattern generator of DLPC343x.
Is the data that is configured by the test pattern generator transferred to the DMD as-is without…
Hello Jack,
You mentioned your custom board is using (dlpc3438+dlpa3005+dlp4710), is this a typo for DLPC3438? If you are using DLPC3438, then it will not work with the FWSel_DLPC3439_DLPA3005_SeriesLED_pm1_i2c0x36_v7p7p1.img.
If you are using DLPC3439…
Hello Eugene,
I recommend you try contacting Asia Optics (manufacturer of the DMD optical engine for this EVM) to get more information on the flex cable for this design.
I hope this helps.
Best Regards,
Philippe Dollo
Part Number: DLPC3438 Other Parts Discussed in Thread: DLPA2005 , DLPA2000 , , DLPC3433 Tool/software: Linux in my systems, we use DLPC3438CZEZ / DLPA2000DYFFR and DLP3010FQK.
we use the same option between DLPC and dmd to DLPDLCR3010EVM.
as you know,DLPDLCR3010EVM…
Hi Jimmy,
To confirm, you have an original DLP3010EVM (not G2 version)? If so, this product is End-of-Life and has been superseded by the DLP3010EVM-G2. For such reason and numerous changes made between both systems, the original firmware is no longer…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPC3435 , DLPC3438 , DLPC3433 , DLPC3432 , USB2ANY Hi,
I'm trying to send the video signal to our custom board with DLPC3430. However, there is nothing change with the image.
It remains the original…
Part Number: DLPA3005 Other Parts Discussed in Thread: DLP3010 , DLPC3438 , DLPA3000 , , DLPDLCR3010EVM-G2 Hello,
I have a driver board( dlpa3000+dlpc3438+dlp3010, 280lm), now I want to make the dlp much higher( maybe 25% higher other than 100% higher)…
Hello Chase,
Overall, the DLP3010 and DLP3010LC are not compatible. While the pin-to-pin is identical, they require different controllers. The DLP3010LC requires the DLPC3478 whereas the DLP3010 requires the DLPC3438. The firmware is different as well…