Part Number: DLPDLCR4710EVM-G2 Other Parts Discussed in Thread: DLPA3005 , DLPC3439 Hi, team,
I found DLPA3005 is not recommended for new design, so which PMIC can be used with DLPC3439? do you have the reference design?
thanks
Part Number: DLPC3439 Dear TI,
Reading the documentation DLPU035 (Programmer's Guide of DLPC3439), you are refering to the command "Write Manual Duty Cycle Select" (note 5 - page 52).
I didn't found this command elsewhere in this guide.…
Part Number: DLPDLCR4710EVM-G2 Other Parts Discussed in Thread: DLPC3439 , DLP4710EVM-LC
Hello,
I have a problem with DLPDLCR4710EVM-G2, it is not running. How do I get fixed? Or is it defective?
Part Number: DLPC3439 Hi, how can I change pixel clock capture edge from rising edge (default setting) to falling edge ? In the DLP3439 datasheet is noticed that active capture edge of PCLK is software programmable. I see configuration command only for…
Part Number: DLPC3439 Other Parts Discussed in Thread: DLP4710 , , DLPC3433 , DLPC3438 Hi,
In the Programmer's Guide DLPU035 related to the DLPC3439 controller, it is mentionned (page 59 of the document) the possibility to operate the DLP4710 chipset in…
Part Number: DLP4710 Other Parts Discussed in Thread: , DLPC3439 , DLPC3479 We are now developing one UV light engine for 3D printer, and we use the DLP4710 in our UV light engine and the UV LED is 385nm. We already run the life cycle test one year (the…
Part Number: DLPC3439 Other Parts Discussed in Thread: DLP4710 , DLPC3479 , DLPC350 Hi,
If I set the display resolution to 1920 x 1080 using the command "Write Display Size", and the video input resolution to 1920 x 1080 using the command "Write External…
Part Number: DLP4710 Other Parts Discussed in Thread: DLPC3439 , DLPDLCR4710EVM-G2 Hello, TI Experts,
Our customer sent us a questions about DLP4710 with dual DLPC3439 control.
Question:
Which pixels are controlled by each DLPC3439?
- One DLPC controls…
Part Number: DLPC3439 Other Parts Discussed in Thread: DLP4710 , , DLPA3000 Hello Team, I have a customer with the following inquiry below,
"Could you provide help to understand how to create the contents for the SPI PROMS attached to the DLPC3439 chips…