Part Number: DLP4710LC Other Parts Discussed in Thread: DLPC3479 , DLPA3005
Tool/software:
Dear TI experts
We have a design based on your components for integration into our application of several thousand installations per year. We designed our custom…
Part Number: DLPC3479 Other Parts Discussed in Thread: DLP4710EVM-LC
Tool/software:
When I write device address 8 'h36, dlpc3479 has an ack signal. But when I wrote to the register address, dlpc3479 did not have an ack signal, resulting in a failure…
Part Number: DLPC3479 Other Parts Discussed in Thread: DLPA3005 , DLP4710EVM-LC Tool/software: When I set 00h to 5Bh using the DLPC3479's "Write RGB LED Current PWM (54h)" command and read it back, the set value becomes 5Bh. Why is that? …
Part Number: DLPC3479 Other Parts Discussed in Thread: DLP4710LC , , DLPA3005 Tool/software: Hello! I'm using External Pattern Mode, 8-bit monochrome patterns。 I'm uses the PARALLEL RGB interface, the timing is RGB888, and the external input is 1920…
Part Number: DLPC3479
Tool/software:
Dear
I am checking the TI's EVM schematic to make our hardware.
Q1) All GPIOs&TSTPs have an I/O voltage level of 1.8 V.
Although the 3.3 V power selection resistor is DNI (Do Not Install), looking at the TI…
The issue where the PAT_RDY signal fails even when PROJ_ON is provided, with a failure rate of about 1 in 500 times, could be due to several factors. One possibility is a timing or communication issue between the DLPC3479 controller and…
Part Number: DLPC3479 Other Parts Discussed in Thread: DLP4710LC , , DLPA3005 Tool/software: Hello! I'm using External Pattern Mode, 8-bit monochrome patterns。 I'm uses the PARALLEL RGB interface, the timing is RGB888, and the external input is 1920…
Part Number: DLPC3479 Other Parts Discussed in Thread: DLP4710LC , , DLPA3005 Tool/software: Hello!
I use a self-made board, the hardware structure is dlp4710lc + dlpc3479 + dlpa3005.
When the Display - External Video Mode is used (05 register is set to…
Hello,
This thread is being duplicated and the original question has been resolved as the DLP4710LC is displaying an image.
Kindly accept resolution of this thread and the other questions will be resolved in other threads here:
https://e2e.ti.com/support…
Part Number: DLPC3479 Other Parts Discussed in Thread: DLPA3005 , DLP4710LC Tool/software: Hello, We used DLPC3749+DLP4710LC+DLPA3005 to make 10 prototypes and found that half of the machines showed misalignment between the left and right projections when…