Part Number: DLPC410 Hi,
I've just got the Discovery DLP4100 Kit that has the DLPC410 Chipset, I have followed the installation process and every time I go to update the driver the folders only have Windows 7/8/10 but like I said I'm running Windows…
Richard,
Sorry for the delay, I had to look into this a bit.
There is nothing on the board to set. However, in the software, please make sure you are selecting the right platform cable and set it as JTAG.
I would recommend backing up the default…
Part Number: DLPC410 Other Parts Discussed in Thread: DLPLCRC410EVM Hello,
I would like to consult on the matter below: In the DLPC410 datasheet (DLPS024G –AUGUST 2012–REVISED FEBRUARY 2020), for PWR_FLOAT pin, it is stated that: "Connected to output…
Part Number: DLPC410 Other Parts Discussed in Thread: DLPC900 , Hello.
I would like to know how DLPC410 and DLPC900 perform PWM to show, for example, an 8-bit grayscale image.
The micro-mirror need to change between 0 and 1 according with some time…
Part Number: DLPC410
Hello, In the DLPC410 datasheet this signal is stated as active high, meaning, once the DLPR410 finished to load it will go high (page 14 in the DS)
but later on on page 61 (section 9.3 - Initialization Setup) it is stated that…
Part Number: DLPC410 Hello,
Upon startup the D2 LED is red and remains red unless I connect the board via usb to the Discovery 4100 GUI and wait for the D4100_GUI_FPGA.bin to programmed at which point D2 turns off and D16 turns green. As user "Fizix…
Part Number: DLPC410 Other Parts Discussed in Thread: DLPLCRC410EVM Hello,
I design a board with the DLPC410 which controls DMD at data rate of 800Mbps.
My question is regarding the DLPC410 Ref Clock: " CLKIN_R ".
According the datasheet - "The…
Part Number: DLPC410 Hi team,
We have a customer inquiring about DLPCRC410EVM,Below is the verbatim of his inquiry.
"I want to use dlpcrc410evm ( https://www.ti.com/tool/DLPLCRC410EVM ) to achieve a 22kHz refresh rate, so I started to understand the…
Part Number: DLPC410 Hello,
My coworker purchased a DLPRC410EVM for a research project. I purchased a 5V, 6amp power supply. I followed the directions on the manual precisely to turn it on, but nothing would power. No LEDs were triggered, even after…