Part Number: DLPC4422-SW Other Parts Discussed in Thread: DLPC4422 Tool/software: As the tittle description
How to skip the blanking scene of the Dual DLPC4422 from external to solid field when plugging out HDMI cable? Is any method to disable DLPC4422…
Part Number: DLPC4422-SW Tool/software: Hi,
after installing the application & driver as described, I receive the error message "the application has failed to start because its side-by-side configuration is incorrect" on two different PCs (Win10 & 11…
Part Number: DLPC4422-SW Hi TI,
I tried several time to install DLPC4422GUI using, for example, the link below:
http://www.ti.com/tool/DLPC4422-SW
The file is downloading without problem and I can launch the installation (screenshot below).…
Marvin,
Yes, for now refer to the DLPC4422 Programmer's Guide. You can also refer to the Programmer's Guides that are included in the DLP470TE and DLP660TE SW Downloads.
NOTE: The DLPC4422 binaries will NOT run on the DLPC4420; however the software…
Part Number: DLP660TE-SW Other Parts Discussed in Thread: DLP660TE , DLPC4422 Hi TI Engineer,
When using DLPDLCR660TEVM and DLPLCRDC4422EVM development board, We want to add XPR function.
Use environment
Hardware: DLPDLCR660TEVM ,DLPLCRDC4422EVM…
Part Number: DLP660TE-SW Other Parts Discussed in Thread: DLP660TE , DLPC4422
Hi TI engine,
When using DLPDLCR660TEVM and DLPLCRDC4422EVM development board, We encountered some problems in use.
Use environment
Hardware: DLPDLCR660TEVM…
Alpesh,
The EVM does not require a "front end" to run. For internal development and bench work, we control the projector over USB via the DLPC4422 GUI (Windows). This GUI can be downloaded here: https://www.ti.com/tool/DLP660TE-SW . One needs the DLPC4422…
Part Number: DLPDLCR660TEVM Other Parts Discussed in Thread: DLP660TE , DLPC4422 Hi Team, seeking some support for a customer.
I have a front board that converts the input select (HDMI) to Vx1. The FPGA_CONF (D10) and Vby1_LOCK (D1) indicators are…
Mark,
Can you clarify what it is that you are looking for? Are you looking to display an arbitrary test pattern from within the DLPC4422 EVM firmware, without using an external Vx1 input? If so, that capability does not currently exist in the TI.com…
Jonathan,
The supported Vx1 input timings for the EVM are listed in an xls file include in the DLP660TE-FW download. https://www.ti.com/tool/DLP660TE-SW
Please note that the supported Vx1 input timings are very limited (600MHz pixel clock only): …