Part Number: DLPC6401 Hi,
I am working on DLP display project. We used an DLPC6401 as DLP Data Processor.
A parallel flash memory is connected on it. I want to install the firmware into the flash by I2C1 interface via the DLPC6401 GUI 1.0 tool.
I receive…
Part Number: DLPC6401 Other Parts Discussed in Thread: SN65DSI83 , Hello,
We have designed in Home Appliance Product in which we have interfaced "DLPC6401" with "SN65DSI83"(DSI To Single Channel FPD Link LVDS Bridge).
We have following…
Part Number: DLPC6401
Hi there,
I am able to communicate with the DLPC6401 using an Arduino UNO .
What I'd like to do is an offset of the displayed resolution.
In the datasheet, it seems to be associated to the Display Position in Frame register at address…
Part Number: DLPC6401 The Front is Mstar U69 ouput lvds (1280*800 60hz clock 83.5Mhz ) and the back TI DLPC6401 lvds input .
Now the problem is DLPC6401 can not detect lvds input data, the blow is Debug message:
Event: Source No Syncs on channel
I have…
Hello Nilesh,
I'm not familiar with the DLPC6401 video parameters. Please, post your question of the DLPC6401 in the Video and Data Display > DLP Video and Data Forum.
I suggest you using DSI Tuner to configure the SN65DSI83 based on the parameters…
Part Number: DLPC6401 Other Parts Discussed in Thread: DLP4500 , Hi,
I have a question about synchronization of input and output images. When using DLPC6401 for DLP4500, what is the delay of the output image relative to the input source?
Best regards, H.…
Part Number: DLPC6401 Other Parts Discussed in Thread: DLP4501 , DLP4710 , DLP3010 , DLPC350 I need a video processing front end to support input from the relatively new HDMI 2 standard. The requirements are 1) Support of 1080p signal at 60Hz 2) Support of…
Hello
As described in the layout guidelines the maximum length of the DDR interface signal is about 100 mm.
Is there any mean to allow a maximal length up to 2 meters between the DLP and the DMD? Perhaps using serdes or somethingh like that.
As anyone…
Other Parts Discussed in Thread: DLPC6401 Hello
I am programming at the moment an interface for the DLPC6401 using the I2C.
I want to reduce the LED current to reduce the brightness. But at the moment I can change the values, but there is no influence…