Hi Sanjeev,
When keystone function is off, the video signal loop through FPGA to DLPC6421 directly, or FPGA need to do some calculation in DDR3?
Geoffrey
Part Number: DLPC6421 Hi Sirs,
I want to add a Flash into composer FlashDeviceParameters
Can you provide the parameters setting?
MX29LV320EBTI-70G
Thanks.
Geoffrey
Part Number: DLPC6421 Hi Sir,
I saw DLPC6421 Software Programmer’s Guide mentioned there is reference source code. Where can I get this reference source code?
thank you.
best regards,
Langston
Part Number: DLPC6421 Hi sir,
We are designing a 4K projector using DLPC6421 x 2. I'm curious how keystone work with DLPC6421.
- I know there is I2C command to enable/disable keystone.
- do we need to add tilt sensor to calculate degree first? how…
Part Number: DLPC6421DLPC6421 connected to DMD DLP470TP.
When booting, debugging message shown below.
Could anyone give hint of the possible problem? Is my DMD LVDS bus has problem?
"......
PAD Rev ID = 3
sysmon: Low-power mode change cc = 1
sysmon…
Part Number: DLPC6421 the latest dlpc6421 datasheet has a duplicate pinnumber AE19
last row on page5 has pin p1_c_4 at AE19
then the 4th row on the next page for pin p1_c_0 on the next page also says AE19
Can someone provide the correct pinNumbers for…
Part Number: DLPC6421 I submitted datasheet feedback, but I need to know the
proper pin numbers for
P1_C_4
P1_C_0
as soon as possible
I thought I submitted this same question yesterday, but I could not find it in the search for questions raised by me…
Part Number: DLPC6421 Hi TI, I've got a pair of Optotune XPR-25 shifters that I need to drive and would like to order some samples of the EVM Driver board that controls them. Two, to be precise. It is for a prototype display.
Can you tell me what…
Hi Matt
Glad to See You Again
Discuss the control mode of XPR and number of channels
A. DAC mode or PWM mode
B. 2-Way or 4-Way
Who is using DAC mode
A. DLPC4422EVM + DLP660TEEVM is using DAC mode and 2-Way
B. DLPC4422EVM + DLP470TEEVM is using DAC mode…